<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can we use high-speed on FRDM K64 with additionnal chips in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040424#M56771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to know if the FRDM K64 which is using only full-speed USB could work with high-speed chips like the Texas instrument TUSB216RWBT.&lt;BR /&gt;If yes, will it be possible to increase the speed.&lt;/P&gt;&lt;P&gt;Thank you for your help in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2020 22:14:10 GMT</pubDate>
    <dc:creator>flauberttagu</dc:creator>
    <dc:date>2020-07-13T22:14:10Z</dc:date>
    <item>
      <title>Can we use high-speed on FRDM K64 with additionnal chips</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040424#M56771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to know if the FRDM K64 which is using only full-speed USB could work with high-speed chips like the Texas instrument TUSB216RWBT.&lt;BR /&gt;If yes, will it be possible to increase the speed.&lt;/P&gt;&lt;P&gt;Thank you for your help in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 22:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040424#M56771</guid>
      <dc:creator>flauberttagu</dc:creator>
      <dc:date>2020-07-13T22:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use high-speed on FRDM K64 with additionnal chips</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040425#M56772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 Yes.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115686i3BD46905954FB84B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2 No.&amp;nbsp;Full-speed and low speed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115687i837B61AF77E4C900/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------- &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 00:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040425#M56772</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-07-14T00:47:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use high-speed on FRDM K64 with additionnal chips</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040426#M56773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Da Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Excellent day !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 09:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040426#M56773</guid>
      <dc:creator>flauberttagu</dc:creator>
      <dc:date>2020-07-14T09:12:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use high-speed on FRDM K64 with additionnal chips</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040427#M56774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K64 can only be used for low or full-speed USB device/host/OTG. To use it at high speed an external HS USB controller would be needed (eg. via SPI).&lt;BR /&gt;If your design needs HS USB operation it is simpler to move to the K65/K66 instead, which then allows one low/full speed OTG interface plus one low/full/high speed one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jul 2020 10:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1040427#M56774</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-07-19T10:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use high-speed on FRDM K64 with additionnal chips</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1160533#M58301</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it possible to move easily from a code develop for the K64 to the K65 or K66? Are those two ARM compatible to K64 in terms of computing?&lt;/P&gt;&lt;P&gt;Thx is andvance.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 08:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-high-speed-on-FRDM-K64-with-additionnal-chips/m-p/1160533#M58301</guid>
      <dc:creator>flauberttagu</dc:creator>
      <dc:date>2020-09-29T08:32:02Z</dc:date>
    </item>
  </channel>
</rss>