<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Software breakdown on interrupt?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Software-breakdown-on-interrupt/m-p/1039659#M56769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I´m new with the Kinetis Controllers and I get a problem with the Interrups.&lt;/P&gt;&lt;P&gt;I´m using the IAR Workbenck and a Jlink programmer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I put my software on an MKL03Z8VFG4 every time a interrupt is triggert the controller jumps to an not used flash adress.&lt;/P&gt;&lt;P&gt;I have check with the TMP0, TMP1, LPTMP0 and the ADC interrupt.&lt;/P&gt;&lt;P&gt;If the interrupt is not triggert the programm work fine.&lt;/P&gt;&lt;P&gt;The same Software on the FRDM-KL03Z Board have no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check the map file and see the IQR Handler on the correct position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have somebody an idea about this problme?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Apr 2020 07:06:22 GMT</pubDate>
    <dc:creator>harms_matthias8</dc:creator>
    <dc:date>2020-04-01T07:06:22Z</dc:date>
    <item>
      <title>Software breakdown on interrupt?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Software-breakdown-on-interrupt/m-p/1039659#M56769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I´m new with the Kinetis Controllers and I get a problem with the Interrups.&lt;/P&gt;&lt;P&gt;I´m using the IAR Workbenck and a Jlink programmer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I put my software on an MKL03Z8VFG4 every time a interrupt is triggert the controller jumps to an not used flash adress.&lt;/P&gt;&lt;P&gt;I have check with the TMP0, TMP1, LPTMP0 and the ADC interrupt.&lt;/P&gt;&lt;P&gt;If the interrupt is not triggert the programm work fine.&lt;/P&gt;&lt;P&gt;The same Software on the FRDM-KL03Z Board have no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check the map file and see the IQR Handler on the correct position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have somebody an idea about this problme?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2020 07:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Software-breakdown-on-interrupt/m-p/1039659#M56769</guid>
      <dc:creator>harms_matthias8</dc:creator>
      <dc:date>2020-04-01T07:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: Software breakdown on interrupt?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Software-breakdown-on-interrupt/m-p/1039660#M56770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/harms.matthias84@googlemail.com"&gt;harms.matthias84@googlemail.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you modify the VTOR register? If this register doesn't have the address of your vector interrupt this could be the reason the program is jumping to other flash locations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2020 12:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Software-breakdown-on-interrupt/m-p/1039660#M56770</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-04-10T12:59:34Z</dc:date>
    </item>
  </channel>
</rss>