<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK60DN512VLL10 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10/m-p/238812#M5676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Am looking for information on what are the minimum&lt;BR /&gt;requirements for this chip. I'm also looking for the programming options and&lt;BR /&gt;debugging options. It appears on the evaluation board that they are using a JM&lt;BR /&gt;60 chip through USB to do the debugging. Is this the only option? The project&lt;BR /&gt;I'm working on is very small so the component count is critical. Any and all&lt;BR /&gt;help would be very appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Sep 2013 11:10:44 GMT</pubDate>
    <dc:creator>danostrander</dc:creator>
    <dc:date>2013-09-18T11:10:44Z</dc:date>
    <item>
      <title>MK60DN512VLL10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10/m-p/238812#M5676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Am looking for information on what are the minimum&lt;BR /&gt;requirements for this chip. I'm also looking for the programming options and&lt;BR /&gt;debugging options. It appears on the evaluation board that they are using a JM&lt;BR /&gt;60 chip through USB to do the debugging. Is this the only option? The project&lt;BR /&gt;I'm working on is very small so the component count is critical. Any and all&lt;BR /&gt;help would be very appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2013 11:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10/m-p/238812#M5676</guid>
      <dc:creator>danostrander</dc:creator>
      <dc:date>2013-09-18T11:10:44Z</dc:date>
    </item>
  </channel>
</rss>