<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 2 ways traffic light with pedestrian crossing button traffic light in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/2-ways-traffic-light-with-pedestrian-crossing-button-traffic/m-p/1032289#M56559</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are some examples in the SDK, you can download it in this link: &lt;A href="https://mcuxpresso.nxp.com/en/builder"&gt;SDK Builder&lt;/A&gt;. Choose the FRDM-KL25Z board, select the IDE, in your case Keil MDK, and add all the middleware options so you can see all the examples.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96534i62492DCC526173BD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For your specific application, there is an example you can check . See the gpio_led_output driver example, so you can see how to configurate a led. A button configuration for your application is also with the GPIO, but in this case it is an input (which in the led was an output).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You also can see the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL25P80M48SF0RM.pdf"&gt;Reference Manual&lt;/A&gt; for more information of the peripherals configuration. The GPIO chapter is the 41, where you can see the Registers Configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 23:14:47 GMT</pubDate>
    <dc:creator>nxf58474</dc:creator>
    <dc:date>2019-12-11T23:14:47Z</dc:date>
    <item>
      <title>2 ways traffic light with pedestrian crossing button traffic light</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/2-ways-traffic-light-with-pedestrian-crossing-button-traffic/m-p/1032288#M56558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi everyone sir,i'm needed help because don't know Using the FRDM-KL25Z board, with uVision 5 Keil compiler. 2 ways traffic light with pedestrian crossing button traffic light program. C programming&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;leong&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 03:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/2-ways-traffic-light-with-pedestrian-crossing-button-traffic/m-p/1032288#M56558</guid>
      <dc:creator>jordanliong95</dc:creator>
      <dc:date>2019-12-11T03:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: 2 ways traffic light with pedestrian crossing button traffic light</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/2-ways-traffic-light-with-pedestrian-crossing-button-traffic/m-p/1032289#M56559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are some examples in the SDK, you can download it in this link: &lt;A href="https://mcuxpresso.nxp.com/en/builder"&gt;SDK Builder&lt;/A&gt;. Choose the FRDM-KL25Z board, select the IDE, in your case Keil MDK, and add all the middleware options so you can see all the examples.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96534i62492DCC526173BD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For your specific application, there is an example you can check . See the gpio_led_output driver example, so you can see how to configurate a led. A button configuration for your application is also with the GPIO, but in this case it is an input (which in the led was an output).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You also can see the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL25P80M48SF0RM.pdf"&gt;Reference Manual&lt;/A&gt; for more information of the peripherals configuration. The GPIO chapter is the 41, where you can see the Registers Configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 23:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/2-ways-traffic-light-with-pedestrian-crossing-button-traffic/m-p/1032289#M56559</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2019-12-11T23:14:47Z</dc:date>
    </item>
  </channel>
</rss>