<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KW41Z waken up by unknown reason</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-waken-up-by-unknown-reason/m-p/1031739#M56541</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;KW41Z Wake up problem&lt;/P&gt;&lt;P&gt;I am developing an application about transfering data via BLE 4.0 using KW41Z board. I am quite successful to do so but the app only works correctly within some minutes.&lt;/P&gt;&lt;P&gt;I set connection event period of BLE: 2s.&lt;/P&gt;&lt;P&gt;I used LPTMR to hardware trigger ADC 16bit. When ADC conversion completes, it triggers DMA to move data from ADC result register to a defined area of memory. LPTMR period: 20ms, DMA interupts MCU after 200 ADC conversions (4s).&lt;/P&gt;&lt;P&gt;MCU works at VLPS mode when it is not interrupted by DMA or BLE thread. Everything is fine until an unknown source wakes MCU up and it seems to be weird that DMA interrupt and BLE connection interrupt still work and at the end of ISR of these interrupt I put "PWR_AllowDeviceToSleep();" function that I want MCU to come back to VLPS mode but IT DOES NOT WORK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I must mention that I control every other sources of the interrupt and facilitate not to let these interruption happen.&lt;/P&gt;&lt;P&gt;I use an instrument that can record Board current. As you can see in the attached image, after normal running, at 08:26 power increases and never goes down. It means MCU gets out of VLPS mode and never comes back.&lt;/P&gt;&lt;P&gt;Can anybody give me any advice? I will much appreciate it. Thank you very much in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Feb 2020 12:02:18 GMT</pubDate>
    <dc:creator>micheal_hoang_b</dc:creator>
    <dc:date>2020-02-14T12:02:18Z</dc:date>
    <item>
      <title>KW41Z waken up by unknown reason</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-waken-up-by-unknown-reason/m-p/1031739#M56541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;KW41Z Wake up problem&lt;/P&gt;&lt;P&gt;I am developing an application about transfering data via BLE 4.0 using KW41Z board. I am quite successful to do so but the app only works correctly within some minutes.&lt;/P&gt;&lt;P&gt;I set connection event period of BLE: 2s.&lt;/P&gt;&lt;P&gt;I used LPTMR to hardware trigger ADC 16bit. When ADC conversion completes, it triggers DMA to move data from ADC result register to a defined area of memory. LPTMR period: 20ms, DMA interupts MCU after 200 ADC conversions (4s).&lt;/P&gt;&lt;P&gt;MCU works at VLPS mode when it is not interrupted by DMA or BLE thread. Everything is fine until an unknown source wakes MCU up and it seems to be weird that DMA interrupt and BLE connection interrupt still work and at the end of ISR of these interrupt I put "PWR_AllowDeviceToSleep();" function that I want MCU to come back to VLPS mode but IT DOES NOT WORK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I must mention that I control every other sources of the interrupt and facilitate not to let these interruption happen.&lt;/P&gt;&lt;P&gt;I use an instrument that can record Board current. As you can see in the attached image, after normal running, at 08:26 power increases and never goes down. It means MCU gets out of VLPS mode and never comes back.&lt;/P&gt;&lt;P&gt;Can anybody give me any advice? I will much appreciate it. Thank you very much in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 12:02:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-waken-up-by-unknown-reason/m-p/1031739#M56541</guid>
      <dc:creator>micheal_hoang_b</dc:creator>
      <dc:date>2020-02-14T12:02:18Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z waken up by unknown reason</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-waken-up-by-unknown-reason/m-p/1031740#M56542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phuoc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to confirm, how are you transferring&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;data via BLE 4.0? The kw41 supports Bluetooth LE 4.2.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;What is the example that you are working on? I recommend the Heart Rate Sensor or the temperature sensor to a better reference for the sleep mode that the device supports with Bluetooth LE.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Mario&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 21:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-waken-up-by-unknown-reason/m-p/1031740#M56542</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2020-02-17T21:35:17Z</dc:date>
    </item>
  </channel>
</rss>