<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Need Application note on K60 ENET Module.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-Application-note-on-K60-ENET-Module/m-p/1029602#M56479</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Download the open source version of the uTasker project from GITHUB and follow this tutorial: &lt;BR /&gt;&lt;A href="https://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis.pdf" target="test_blank"&gt;https://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It runs a simulated Kinetis part with its Ethernet module so you can do both practical tests and step through the code to see how the Ethernet module operates (how it is configured, controlled and how it works internally - address filltering, interrupt generation, buffer copying and so on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Feb 2020 21:48:52 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-02-15T21:48:52Z</dc:date>
    <item>
      <title>Need Application note on K60 ENET Module.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-Application-note-on-K60-ENET-Module/m-p/1029601#M56478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am New in Ethernet protocol implementation or network protocol implementation. I read ENET Module chapter in K60 Manual, but i need more details information on ENET Module. So, please suggest any Application Note on K60 ENET Module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nandish Jasani.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 04:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-Application-note-on-K60-ENET-Module/m-p/1029601#M56478</guid>
      <dc:creator>nbjasani</dc:creator>
      <dc:date>2020-02-14T04:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: Need Application note on K60 ENET Module.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-Application-note-on-K60-ENET-Module/m-p/1029602#M56479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Download the open source version of the uTasker project from GITHUB and follow this tutorial: &lt;BR /&gt;&lt;A href="https://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis.pdf" target="test_blank"&gt;https://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It runs a simulated Kinetis part with its Ethernet module so you can do both practical tests and step through the code to see how the Ethernet module operates (how it is configured, controlled and how it works internally - address filltering, interrupt generation, buffer copying and so on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Feb 2020 21:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-Application-note-on-K60-ENET-Module/m-p/1029602#M56479</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-02-15T21:48:52Z</dc:date>
    </item>
  </channel>
</rss>