<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis K64 CAN communication in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029093#M56446</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thank you very much but&amp;nbsp;unfortunately I can't use uTasker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Mar 2020 15:38:08 GMT</pubDate>
    <dc:creator>LArmstrong1985</dc:creator>
    <dc:date>2020-03-14T15:38:08Z</dc:date>
    <item>
      <title>Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029091#M56444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;BR /&gt;starting from the example fdrmk64f_flexcan_loopback I made two programs, one transmitter and one receiver, installed on two boards&amp;nbsp;connected via two TJA1050 transceivers. Signals seem ok,&amp;nbsp;but the interrupt does not trigger on the receiver.&lt;/P&gt;&lt;P&gt;The changes I made are the following:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;in both software I setted&amp;nbsp;flexcanConfig.enableLoopBack to false&lt;/P&gt;&lt;P&gt;- in both software I configured CAN0 to pin PTB18 and PTB19 on pinmux&lt;/P&gt;&lt;P&gt;- on trasmitter I removed receive mb configuration and receive interrupts&lt;/P&gt;&lt;P&gt;- on receiver I removed transmitter mb configuration&lt;/P&gt;&lt;P&gt;Can you take a look to find out if I did well or is there something wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 08:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029091#M56444</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2020-03-13T08:57:21Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029092#M56445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Take a look at &lt;A href="https://www.utasker.com/docs/uTasker/uTaskerCAN.PDF" target="test_blank"&gt;https://www.utasker.com/docs/uTasker/uTaskerCAN.PDF&lt;/A&gt;&lt;BR /&gt;and&lt;BR /&gt;&lt;A href="https://www.youtube.com/watch?v=Ha8cv_XEvco" target="test_blank"&gt;https://www.youtube.com/watch?v=Ha8cv_XEvco&lt;/A&gt;&lt;BR /&gt;It is available in the open source uTasker project on all Kinetis processors with FlexCAN.&lt;BR /&gt;It allows the FlexCAN to be simulated and easily investigated to help solve problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 12:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029092#M56445</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-03-13T12:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029093#M56446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thank you very much but&amp;nbsp;unfortunately I can't use uTasker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2020 15:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029093#M56446</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2020-03-14T15:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029094#M56447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As noted, the uTasker project can be used as "working reference" to solve problems with environments that don't yet work but are specified to be used. &lt;EM&gt;Its simulation capability is very useful in understanding how the code flow and the register settings should be. Since it is free open source there should be no objections from finance departments or developments on a shoe-string either.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2020 02:41:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029094#M56447</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-03-16T02:41:13Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029095#M56448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I attached the decoded signal that I received and it is correct. However, it still does not trigger any interrupt in reception.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;The doubts I have from the beginning looking at the example are the following&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;where is setted the CAN ID of each individual board? From the example it seems that it can be set only in the messages in transmission and in reception therefore each card can send and receive messages with different IDs. It's correct?&lt;/P&gt;&lt;P&gt;- the ID entered in the txframe is that of the transmitter or that of the recipient of the message? Same question for the receiver: the ID entered in rxframe is that of the transmitter to be listened to or that of the receiver?&amp;nbsp;In my separate examples for transmitter and receiver I left the same id value in the txframe and in the rxframe that is 0x123&lt;/P&gt;&lt;P&gt;- Through the logical analyzer I see that the message is repeated several times even if it is sent only once in the example.&lt;BR /&gt;Why? Is it the CAN controller that sends back if there is no answer?&lt;/P&gt;&lt;P&gt;- In the original example CAN RX and TX pin were not configured. That is the configuration that I added in MCUXpresso Config Tool. Is OK?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100429i6F4E04CCB24980EB/image-size/large?v=v2&amp;amp;px=999" title="CAN configuration.JPG" alt="CAN configuration.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- The last doubt is on the transceiver that I used, the TJA1050. I looked that I needed 5V on VCC.&amp;nbsp;I think the signal is still 3.3v as it is generated by MCU.&amp;nbsp;Could it be that it is not compatible as a transceiver?&lt;/P&gt;&lt;P&gt;I hope you can help me!&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99284iB92ECC08801D263A/image-size/large?v=v2&amp;amp;px=999" title="CAN_RX_SIGNAL.JPG" alt="CAN_RX_SIGNAL.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2020 09:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029095#M56448</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2020-03-24T09:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029096#M56449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved.&amp;nbsp;The problem was that the frdmk64_interrupt_loopback example had to do only with Message Buffers.&lt;/P&gt;&lt;P&gt;By configuring CAN TX and RX pins and disabling the loopback, most likely, however, it was transmitting but was not enabled to receive.&amp;nbsp;I found another example, specifically&amp;nbsp;twrk64f120m_flexcan_interrupt_transfer and all works well.&lt;/P&gt;&lt;P&gt;Now I have some doubts about how to configure the CAN module to receive from multiple transmitters.&lt;/P&gt;&lt;P&gt;Do I have to configure a message buffer for each ID I want to manage?&lt;/P&gt;&lt;P&gt;And if I don't know which IDs can send me data and want to receive from all possible IDs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2020 17:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029096#M56449</guid>
      <dc:creator>LArmstrong1985</dc:creator>
      <dc:date>2020-03-24T17:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 CAN communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029097#M56450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fabio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;i have same issue what you tell above. i have only one board configure as transmitter and i connect the CAN_H through the Transceiver to the CAN analyzer. i also disable the loopback and cinfig the pin mux. then i start debugging but message not send because of program stopped here.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while (0U == FLEXCAN_GetMbStatusFlags(base, u32flag &amp;lt;&amp;lt; mbIdx))&lt;BR /&gt; {&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the flag not set. are you facing this issue or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i attaced the pic for your reference.&lt;/P&gt;&lt;P&gt;I'm using MKV42F microcontroller. i do code with example of&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;frdmk64_interrupt_loopback.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/105733i4E17A94A888354CC/image-size/large?v=v2&amp;amp;px=999" title="can_stop.png" alt="can_stop.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2020 11:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-CAN-communication/m-p/1029097#M56450</guid>
      <dc:creator>senthilprabhug</dc:creator>
      <dc:date>2020-04-09T11:48:24Z</dc:date>
    </item>
  </channel>
</rss>