<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV46 NanoEdge clock</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025382#M56356</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Julien,&lt;/P&gt;&lt;P&gt;I have checked the data sheet of KV4x, I think it is okay to use 84MHz/168MHz as eFlexPWM nano-edge clock source.&lt;/P&gt;&lt;P&gt;This is the copy from data sheet of KV4x reversion 3.&lt;/P&gt;&lt;P&gt;Pls have a try.&lt;/P&gt;&lt;P&gt;Currently, I have not TWER-KV46 board on hand, you can have a try if you have board.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100698i2477C9268261EA08/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 09:23:15 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-02-17T09:23:15Z</dc:date>
    <item>
      <title>KV46 NanoEdge clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025381#M56355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use the NanoEdge module to generate PWM on MKV46F256VLH16 device with 16MHz crystal.&lt;/P&gt;&lt;P&gt;The clock configuration is ambiguous.&lt;/P&gt;&lt;P&gt;In the reference manual, I have found in the clock chapter:&lt;/P&gt;&lt;P&gt;" &lt;EM&gt;The fast peripheral bus clock provides the NanoEdge clock, and MCGPLLCLK provides the "2x Fast peripheral bus clock". Each of these clocks must be an integer divide or multiple of the System clock. The NanoEdge module is expected to be programmed to use clock inputs of 84/168 MHz or 100/200 MHz to support sub-nanosecond resolution control of the flexPWM&lt;/EM&gt;."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But from the PWMA_SMnFRCTRL description :&lt;/P&gt;&lt;P&gt;"&lt;EM&gt;The fractional delay logic can only be used when&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the IPBus clock is running at 100 MHz&lt;/EM&gt;."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The example here (&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-341621"&gt;https://community.nxp.com/docs/DOC-341621&lt;/A&gt;) use 100MHz/200MHz.&lt;/P&gt;&lt;P&gt;If I try to configure the nanoedge 2x clock the same way with the clocks tool of MCUXpresso, it generate an error : "Output frequency must be in range : 164MHz-168Mhz"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Can I use this configuration ?&lt;/P&gt;&lt;P&gt;168MHz Core clock&lt;/P&gt;&lt;P&gt;84MHz Fast peripheral clock&lt;/P&gt;&lt;P&gt;168MHz Nanoedge 2x clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- To use 100MHz/200MHz, is it possible with the clocks tool of MCUXpresso ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Julien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 14:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025381#M56355</guid>
      <dc:creator>jbeaurep</dc:creator>
      <dc:date>2020-02-13T14:23:39Z</dc:date>
    </item>
    <item>
      <title>Re: KV46 NanoEdge clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025382#M56356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Julien,&lt;/P&gt;&lt;P&gt;I have checked the data sheet of KV4x, I think it is okay to use 84MHz/168MHz as eFlexPWM nano-edge clock source.&lt;/P&gt;&lt;P&gt;This is the copy from data sheet of KV4x reversion 3.&lt;/P&gt;&lt;P&gt;Pls have a try.&lt;/P&gt;&lt;P&gt;Currently, I have not TWER-KV46 board on hand, you can have a try if you have board.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100698i2477C9268261EA08/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 09:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025382#M56356</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-02-17T09:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: KV46 NanoEdge clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025383#M56357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;I will not be able to check today. I have not yet received my&amp;nbsp;boards due to the &lt;SPAN style="color: #585858; background-color: #ffffff;"&gt;coronavirus&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;Julien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 13:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-NanoEdge-clock/m-p/1025383#M56357</guid>
      <dc:creator>jbeaurep</dc:creator>
      <dc:date>2020-02-17T13:16:04Z</dc:date>
    </item>
  </channel>
</rss>