<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Use both GPIO and FGPIO</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023447#M56315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand.&lt;BR /&gt;I am always grateful for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Feb 2020 07:42:12 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2020-02-28T07:42:12Z</dc:date>
    <item>
      <title>Use both GPIO and FGPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023445#M56313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am always indebted.&lt;BR /&gt;If I want to use FGPIO in addition to GPIO, do I need to make initial settings such as the direction register of FGPIO if I make initial settings such as the direction register of GPIO?&lt;BR /&gt;Or do I need to configure both if I want to use both GPIOs?&lt;BR /&gt;It seems that only FGPIO should be used, but I also want to use BME, so BME is GPIO based, isn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 05:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023445#M56313</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2020-02-27T05:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: Use both GPIO and FGPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023446#M56314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;FGPIO space is alias to GPIO space. That is writing to FGPIO register also means writing to GPIO register. So, you needn't to write two times.&lt;/P&gt;&lt;P&gt;BME is GPIO based. The peripheral address space occupies a 516 KB region: 512 KB based at 0x4000_0000 plus a 4&lt;BR /&gt;KB space based at 0x400F_F000 for GPIO accesses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2020 04:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023446#M56314</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-02-28T04:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: Use both GPIO and FGPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023447#M56315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand.&lt;BR /&gt;I am always grateful for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2020 07:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-both-GPIO-and-FGPIO/m-p/1023447#M56315</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2020-02-28T07:42:12Z</dc:date>
    </item>
  </channel>
</rss>