<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL26Z 5V Tolerant Inputs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019922#M56246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think it's fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Nov 2019 02:52:10 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-11-25T02:52:10Z</dc:date>
    <item>
      <title>KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019917#M56241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;“The Kinetis Port pins are only 5V tolerant as inputs. The outputs are not 5V tolerant, and that includes pins configured as open-drain outputs. In output mode, if the pin is pulled above VDD, it will cause the output buffer to drive the output at VDD, which will pull-down the pin voltage to near VDD.”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran across this comment in a previous thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to configure a GPIO on the KL26Z we are using as a Hi-Z input (no internal pull up or down) that is externally pulled up to 5V through &amp;gt;20Kohm resistors and then to simulate button presses by turning that GPIO to a low output then back to a Hi-Z input. From the previous comment it seems that this is reasonable if the pins are 5V tolerant as inputs. I wanted to confirm this, or find where I am mistaken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I have scoured KL26 datasheets for the technical data that would support this if confirmed and can’t find any references. Is this documented somewhere?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 18:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019917#M56241</guid>
      <dc:creator>tarikaweimrin</dc:creator>
      <dc:date>2019-11-20T18:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019918#M56242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tarik,&lt;/P&gt;&lt;P&gt;But there is no words say KL26 is 5v tolerant. The max input voltage is 3.6V. Please don't connect 5v signal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 08:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019918#M56242</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-11-21T08:07:42Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019919#M56243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/301393"&gt;Kinetis 5V I2C interface&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the thread posted above it mentions if the GPIO is configured as an input for Kinetis series it would be 5V tolerant.&amp;nbsp; I have this working with no damage on the freedom board for the KL26Z.&amp;nbsp; I see that for the K64 and other in the kinetis series denotes 5V tolerant inputs in datasheets, is the KL26Z different?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 13:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019919#M56243</guid>
      <dc:creator>tarikaweimrin</dc:creator>
      <dc:date>2019-11-21T13:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019920#M56244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;No, not all kinetis have 5v tolerant pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92585iA25986C984FDA8B3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is table 5 in KL26 datasheet.&lt;/P&gt;&lt;P&gt;Yes, I agree pullup through a 20k resistor to 5V can protect the pin. The current is very small. Since there isn't ESD to VDD, there isn't current to VDD also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 03:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019920#M56244</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-11-22T03:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019921#M56245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand it is not recommended.&amp;nbsp; I just want to know if it will cause damage.&amp;nbsp; In the "Off State" as an input with the external resistor there should be little current to damage the chip.&amp;nbsp; In the "On State" the GPIO is configured as a low output.&amp;nbsp;&amp;nbsp;I don't think either state would damage the chip.&amp;nbsp; I just want to see if I am overlooking something.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94638iDFC30579B1DF8819/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 13:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019921#M56245</guid>
      <dc:creator>tarikaweimrin</dc:creator>
      <dc:date>2019-11-22T13:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z 5V Tolerant Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019922#M56246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I think it's fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 02:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL26Z-5V-Tolerant-Inputs/m-p/1019922#M56246</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-11-25T02:52:10Z</dc:date>
    </item>
  </channel>
</rss>