<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 Keil ETM Tracing</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238013#M5621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thought I would add to this thread as I have just had over 4 days faff with the I-Jet Trace probe on the K64 and K24 Tower boards using IAR's Embedded Workbench 7.40.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is what I've found:-&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;1. K64 code examples from both IAR and Freescale assign the wrong port in sysinit.c PTA6,alt7 instead of PTE0,alt5&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;2. The schematics showing port assignment for TRACECLOCKOUT are correct whilst the Tower user manual for the K64 is incorrect&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;3. The Kxx.dmac macro file supplied by IAR is has bugs for the K24 and K64 and most likely others&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P&gt;This info below describes problem/solution for common debugger gotchas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM - 1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Warning - Skipping flash loading pass because there is no data in the&lt;/P&gt;&lt;P&gt;designated range: 0x10000000-0x13FFFFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two flash ranges, 0-0x0FFF FFFF and 0x10000000-0x13FFFFFF&lt;/P&gt;&lt;P&gt;If nothing is placed in one of the ranges then there is a warning that despite being enabled the flash loader was not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION - 1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In Project -&amp;gt; Options -&amp;gt; Debugger -&amp;gt; Download -&amp;gt; Check "Override default .board file" -&amp;gt; delete the line for the surplus&lt;/P&gt;&lt;P&gt;flash range to eliminate the problem, or just ignore this message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM - 2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;ETB trace and SWO cannot co-exist&lt;/P&gt;&lt;P&gt;ETM trace and SWO cannot co-exist.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If ETM or ETB trace is enabled then any SWO data (such as interrupt logging) is sent using the same data channel. IF the board actually allows ETM trace you will with some luck find the correct data being transferred after stopping, but the trace memory is limited, a few million bytes and logging on average one byte per instruction executed, so it fills in seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION - 2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;So if you wish to use any SWO features set trace (Project -&amp;gt; Options -&amp;gt;Debugger -&amp;gt; I-jet -&amp;gt; Trace) to SWO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Trace and SWO to work the latest unreleased Kxx.dmac file is required. This will be released in the next release of EWB (see attached)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following settings get the SWO working on the TWR-K64F120M board:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Changes from the default:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. In Library config: Set library low level interface implementation, stdout/sterr to "via SWO"&lt;/P&gt;&lt;P&gt;2. Set debug driver to I-jet (under download enable Verify download)&lt;/P&gt;&lt;P&gt;3. In I-jet category, set Trace -&amp;gt; 'Trace Data collection' to serial (SWO), disable "Enable ETB"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can see datalog, interrupt and others. I do not want to choke the thin data bus so I do not enable SWO trace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note1:&lt;/P&gt;&lt;P&gt;1. Trace is not supported in hardware on K24 twr, and maybe some others&lt;/P&gt;&lt;P&gt;2. ETM and SWO can not be used at the same time&lt;/P&gt;&lt;P&gt;3. Only SWO will collect data for the timeline display&lt;/P&gt;&lt;P&gt;4. When using any live update feature it is best practice to limit the number of data eg dont have int and data loging on at the same time as there is a limited bandwidth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note2:&lt;/P&gt;&lt;P&gt;Make sure the settings are correct,&lt;/P&gt;&lt;P&gt;1.Library config: Semihosting, via SWO&lt;/P&gt;&lt;P&gt;2.Set debugdriver to I-jet (under download I always enable Verify download)&lt;/P&gt;&lt;P&gt;3.In I-jet category, set Trace Data collection to SWO, disable "Enable ETB"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now SWO data features work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM -3 &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Trace does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K64 supports trace in hardware however TRACECLOCKOUT is routed on chip to PTE0,alt5 but the tower user manual is incorrect as it specifies PTA6, alt7&lt;/P&gt;&lt;P&gt;This is further complicated as all the example code provided by both Freescale and IAR specify PTA6,alt7 in the code examples.&amp;nbsp; This error has also propargated into the Kxx.dmac macro file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;1. Get new Kxx.dmac file from IAR&lt;/P&gt;&lt;P&gt;2. Recode sysinit() in sysinit.c to use PTE0,alt5&lt;/P&gt;&lt;P&gt;3. Make sure settings are correct. see above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lastly, the notes are for the IAR toolchain and probe however I think the same issues are likely to be found in other vendors kit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below are the contents of the Kxx.dmac (I don't know how to upload file so just cut n past and name it Kxx.dmac)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Trace control macro for KinetisK devices&lt;/P&gt;&lt;P&gt;// It has support for ETB (both ETM and ITM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// All global variables are 0 when declared.&lt;/P&gt;&lt;P&gt;// All these variables are prefixed with kinetis_ ...&lt;/P&gt;&lt;P&gt;__var kinetis_etbmodeset;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set to 1 if 'kinetis_etbmode' is set&lt;/P&gt;&lt;P&gt;__var kinetis_etbmode;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Currently set Kinetis ETB mode&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;__var kinetis_calibrate;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Currenlty set calibration value&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Low level write to ETB bits&lt;/P&gt;&lt;P&gt;Kinetis_EnableETB(mask) &lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var value;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var changed;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; bits = 0x3;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; changed = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0xE0043000, "Memory"); // Funnel&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; bits) != mask) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Check if we need to change it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value &amp;amp;= ~bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= mask;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0xE0043000, "Memory");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; changed |= bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0xE0080014, "Memory"); // MCM_ETBCC&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (bits &amp;lt;&amp;lt; 4)) != (mask &amp;lt;&amp;lt; 4)) { // Check if we need to change it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value &amp;amp;= ~(bits &amp;lt;&amp;lt; 4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (mask &amp;lt;&amp;lt; 4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0xE0080014, "Memory");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; changed |= bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = value &amp;gt;&amp;gt; 4;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value &amp;amp;= 0x3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!kinetis_etbmodeset || value != kinetis_etbmode) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Display message, only when mode changes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // This function is called before every 'go/step' and we do not want&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // to see it too often.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_etbmode = value;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_etbmodeset = 1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Display message (so user can see when ETB gets enabled)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x3) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (both ITM and ETM go to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x1) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (only ETM goes to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x2) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (only ITM goes to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB not enabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis_EnableGPIOForETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var value;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var enabled;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; enabled = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0x40048038, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ReadRegister( SIM_SCGC5, &amp;amp;value);&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (1&amp;lt;&amp;lt;13)) == 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (1&amp;lt;&amp;lt;13);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enabling internal clock to Port E&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0x40048038, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // WriteRegister(SIM_SCGC5, value);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; enabled = 1;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0x40048004, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ReadRegister( SIM_SOPT2, &amp;amp;value);&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (1&amp;lt;&amp;lt;12)) == 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (1&amp;lt;&amp;lt;12);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Debug trace clock select = Core/system clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0x40048004, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // WriteRegister(SIM_SOPT2, value);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; enabled = 1;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; // ---- Enabling Trace Pin Function ----&lt;/P&gt;&lt;P&gt;&amp;nbsp; // Trace data and clock pins, high drive strength&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* TRACE CLK and TRACE D0*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D000, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR0,&amp;nbsp; 0x00000700);&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D010, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR4, 0x00000740);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ( __getTracePortSize() &amp;gt;= 2 )&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable TRACE D1*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D00C, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR3,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; } &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ( __getTracePortSize() == 4 )&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable TRACE D2, D3*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D008, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR2,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D004, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR1,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; } &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis_DisableGPIOForETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; // TODO: Reverse actions above (back to defaults)?&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// This is common routine to configure trace on Kinetis&lt;/P&gt;&lt;P&gt;// Kinetis has 2 trace sources (ITM/ETM) and 3 export options (ETM/ETB/SWO).&lt;/P&gt;&lt;P&gt;// The following cases are possible:&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Nothing&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to TPIU (with ITM)&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to ETB, ITM to SWO&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to TPIU, ITM to ETB&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;KinetisConfigureTrace()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var modemask;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var etbena;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; modemask = __getTraceProperty(2);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Get mask of selected modes&lt;/P&gt;&lt;P&gt;&amp;nbsp; etbena&amp;nbsp;&amp;nbsp; = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mask of bits for TPIU&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; if (modemask &amp;amp; 0x6) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ETB (0x4) or SWO (0x2) are allowed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (modemask &amp;amp; 0x2) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Only ETM should go to ETB &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x1 | 0x2;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Both ETM and ITM should go to ETB &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Both ETM and SWO go to TPIU&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; /*Check device for ETB*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; if( __readMemory32(0xE00FF018,"Memory") &amp;amp; 0x1)&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; Kinetis_EnableETB(etbena);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure what goes to ETB&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; if (modemask &amp;amp; 0x10) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Is ETM enabled?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_EnableGPIOForETM();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Yes - enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kinetis_calibrate != 3) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set calibration (only once time)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_calibrate = 3;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (__probeType("JTAGJet"))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __probeCmd("trace calibrate 3");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // For Kinetis calibrate 3 works the best&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_DisableGPIOForETM();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;execConfigureTraceETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!__driverType("ijet")) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Compatible mode (other probes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_EnableGPIOForETM(); // Enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; // This native (ijet) driver (extended functionality)&lt;/P&gt;&lt;P&gt;&amp;nbsp; KinetisConfigureTrace();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Common configuration (for SWO and ETM)&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;execConfigureTraceSWO()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!__driverType("ijet")) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Compatible mode (other probes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Nothing (as it was in original DMAC file).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; // This native (ijet) driver (extended functionality)&lt;/P&gt;&lt;P&gt;&amp;nbsp; KinetisConfigureTrace();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Common configuration (for SWO and ETM)&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MassErase()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (__hasDAPRegs())&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __var mdm_ctrl;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Select bank 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeDPReg(0x01000000, 0x8);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (__readAPReg(0x0) &amp;amp; 0x20)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mdm_ctrl = __readAPReg(0x4) | 0x1;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Do mass erase&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeAPReg(mdm_ctrl, 0x4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Performing mass erase...";&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Wait until finished&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; do&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __delay(100);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; } while(__readAPReg(0x4) &amp;amp; 0x1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase finished";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase is disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase cannot be performed";&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;getPersistentQuickLaunchMacros()&amp;nbsp;&amp;nbsp; // &amp;lt;-- Reserved name, debugger calls it to populate QuickLaunch view.&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __message "getPersistentQuickLaunchMacros";&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var macs;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; macs = "MassErase()";&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; return macs;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2015 08:35:07 GMT</pubDate>
    <dc:creator>DaveTonyCook</dc:creator>
    <dc:date>2015-07-28T08:35:07Z</dc:date>
    <item>
      <title>K60 Keil ETM Tracing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238011#M5619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't manage to get ETM tracing working on my TWR-K60D100M board. I followed the instruction in:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.keil.com/download/files/kinetis_lab.pdf" rel="nofollow noopener noreferrer" title="http://www.keil.com/download/files/kinetis_lab.pdf" target="_blank"&gt;http://www.keil.com/download/files/kinetis_lab.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tracing does not work with the Blinky Example found in Keil Install-Dir: Keil\ARM\Boards\Freescale\TWR-K60N512&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get: "Trace: Data Stream Error", "Trace: Synchronization error",... and no Trace Data is displayed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using my second board, the TWR-K40X256, ETM tracing works perfect:&lt;/P&gt;&lt;P&gt;- same debugger settings&lt;/P&gt;&lt;P&gt;- same trace settings&lt;/P&gt;&lt;P&gt;- corresponding blinky project (TWR-K40X256)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see the TRACE CLK with my oscilloscope: K40: 28MHz, K60: 24MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My settings of the K60 project are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TracePort.ini:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13754454352759821" jivemacro_uid="_13754454352759821"&gt;
&lt;P&gt;FUNC void SetupTrace (void) {
&amp;nbsp; // SIM_SCGC5: enable PORT A clock
&amp;nbsp; _wDWORD(0x40048038,(_RDWORD(0x40048038) | 0x00000200));&lt;/P&gt;
&lt;P&gt;&amp;nbsp; _wDWORD(0x40049018, 0x00000740);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PORTA_PCR6&amp;nbsp; -&amp;gt; (ALT7 + DSE) TRACE_CLKOUT
&amp;nbsp; _wDWORD(0x4004901C, 0x00000740);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PORTA_PCR7&amp;nbsp; -&amp;gt; (ALT7 + DSE) TRACE_D3
&amp;nbsp; _wDWORD(0x40049020, 0x00000740);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PORTA_PCR8&amp;nbsp; -&amp;gt; (ALT7 + DSE) TRACE_D2
&amp;nbsp; _wDWORD(0x40049024, 0x00000740);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PORTA_PCR9&amp;nbsp; -&amp;gt; (ALT7 + DSE) TRACE_D1
&amp;nbsp; _wDWORD(0x40049028, 0x00000740);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PORTA_PCR10 -&amp;gt; (ALT7 + DSE) TRACE_D0
}&lt;/P&gt;
&lt;P&gt;SetupTrace();&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debug: SWJ active, SW, 1MHz&lt;/P&gt;&lt;P&gt;Trace: Core Clock 48MHz, Trace Port Sync Trace Port with 4-bit Data, ETM Trace Enabled, EXCTRC disabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2013 12:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238011#M5619</guid>
      <dc:creator>swtat</dc:creator>
      <dc:date>2013-08-02T12:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: K60 Keil ETM Tracing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238012#M5620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using the K60D100M board you should update your version of Keil, because there are specific examples for it.&lt;/P&gt;&lt;P&gt;Some advanced clock settings are not compatible between K60N512 and K60D100M.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try that first. There may be other causes though.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2013 13:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238012#M5620</guid>
      <dc:creator>paulmartin</dc:creator>
      <dc:date>2013-08-05T13:23:37Z</dc:date>
    </item>
    <item>
      <title>Re: K60 Keil ETM Tracing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238013#M5621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thought I would add to this thread as I have just had over 4 days faff with the I-Jet Trace probe on the K64 and K24 Tower boards using IAR's Embedded Workbench 7.40.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is what I've found:-&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;1. K64 code examples from both IAR and Freescale assign the wrong port in sysinit.c PTA6,alt7 instead of PTE0,alt5&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;2. The schematics showing port assignment for TRACECLOCKOUT are correct whilst the Tower user manual for the K64 is incorrect&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;3. The Kxx.dmac macro file supplied by IAR is has bugs for the K24 and K64 and most likely others&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P&gt;This info below describes problem/solution for common debugger gotchas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM - 1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Warning - Skipping flash loading pass because there is no data in the&lt;/P&gt;&lt;P&gt;designated range: 0x10000000-0x13FFFFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two flash ranges, 0-0x0FFF FFFF and 0x10000000-0x13FFFFFF&lt;/P&gt;&lt;P&gt;If nothing is placed in one of the ranges then there is a warning that despite being enabled the flash loader was not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION - 1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In Project -&amp;gt; Options -&amp;gt; Debugger -&amp;gt; Download -&amp;gt; Check "Override default .board file" -&amp;gt; delete the line for the surplus&lt;/P&gt;&lt;P&gt;flash range to eliminate the problem, or just ignore this message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM - 2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;ETB trace and SWO cannot co-exist&lt;/P&gt;&lt;P&gt;ETM trace and SWO cannot co-exist.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If ETM or ETB trace is enabled then any SWO data (such as interrupt logging) is sent using the same data channel. IF the board actually allows ETM trace you will with some luck find the correct data being transferred after stopping, but the trace memory is limited, a few million bytes and logging on average one byte per instruction executed, so it fills in seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION - 2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;So if you wish to use any SWO features set trace (Project -&amp;gt; Options -&amp;gt;Debugger -&amp;gt; I-jet -&amp;gt; Trace) to SWO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Trace and SWO to work the latest unreleased Kxx.dmac file is required. This will be released in the next release of EWB (see attached)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following settings get the SWO working on the TWR-K64F120M board:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Changes from the default:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. In Library config: Set library low level interface implementation, stdout/sterr to "via SWO"&lt;/P&gt;&lt;P&gt;2. Set debug driver to I-jet (under download enable Verify download)&lt;/P&gt;&lt;P&gt;3. In I-jet category, set Trace -&amp;gt; 'Trace Data collection' to serial (SWO), disable "Enable ETB"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can see datalog, interrupt and others. I do not want to choke the thin data bus so I do not enable SWO trace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note1:&lt;/P&gt;&lt;P&gt;1. Trace is not supported in hardware on K24 twr, and maybe some others&lt;/P&gt;&lt;P&gt;2. ETM and SWO can not be used at the same time&lt;/P&gt;&lt;P&gt;3. Only SWO will collect data for the timeline display&lt;/P&gt;&lt;P&gt;4. When using any live update feature it is best practice to limit the number of data eg dont have int and data loging on at the same time as there is a limited bandwidth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note2:&lt;/P&gt;&lt;P&gt;Make sure the settings are correct,&lt;/P&gt;&lt;P&gt;1.Library config: Semihosting, via SWO&lt;/P&gt;&lt;P&gt;2.Set debugdriver to I-jet (under download I always enable Verify download)&lt;/P&gt;&lt;P&gt;3.In I-jet category, set Trace Data collection to SWO, disable "Enable ETB"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now SWO data features work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PROBLEM -3 &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Trace does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K64 supports trace in hardware however TRACECLOCKOUT is routed on chip to PTE0,alt5 but the tower user manual is incorrect as it specifies PTA6, alt7&lt;/P&gt;&lt;P&gt;This is further complicated as all the example code provided by both Freescale and IAR specify PTA6,alt7 in the code examples.&amp;nbsp; This error has also propargated into the Kxx.dmac macro file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SOLUTION&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;1. Get new Kxx.dmac file from IAR&lt;/P&gt;&lt;P&gt;2. Recode sysinit() in sysinit.c to use PTE0,alt5&lt;/P&gt;&lt;P&gt;3. Make sure settings are correct. see above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lastly, the notes are for the IAR toolchain and probe however I think the same issues are likely to be found in other vendors kit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below are the contents of the Kxx.dmac (I don't know how to upload file so just cut n past and name it Kxx.dmac)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Trace control macro for KinetisK devices&lt;/P&gt;&lt;P&gt;// It has support for ETB (both ETM and ITM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// All global variables are 0 when declared.&lt;/P&gt;&lt;P&gt;// All these variables are prefixed with kinetis_ ...&lt;/P&gt;&lt;P&gt;__var kinetis_etbmodeset;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set to 1 if 'kinetis_etbmode' is set&lt;/P&gt;&lt;P&gt;__var kinetis_etbmode;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Currently set Kinetis ETB mode&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;__var kinetis_calibrate;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Currenlty set calibration value&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Low level write to ETB bits&lt;/P&gt;&lt;P&gt;Kinetis_EnableETB(mask) &lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var value;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var changed;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; bits = 0x3;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; changed = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0xE0043000, "Memory"); // Funnel&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; bits) != mask) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Check if we need to change it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value &amp;amp;= ~bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= mask;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0xE0043000, "Memory");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; changed |= bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0xE0080014, "Memory"); // MCM_ETBCC&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (bits &amp;lt;&amp;lt; 4)) != (mask &amp;lt;&amp;lt; 4)) { // Check if we need to change it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value &amp;amp;= ~(bits &amp;lt;&amp;lt; 4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (mask &amp;lt;&amp;lt; 4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0xE0080014, "Memory");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; changed |= bits;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = value &amp;gt;&amp;gt; 4;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value &amp;amp;= 0x3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!kinetis_etbmodeset || value != kinetis_etbmode) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Display message, only when mode changes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // This function is called before every 'go/step' and we do not want&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // to see it too often.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_etbmode = value;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_etbmodeset = 1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Display message (so user can see when ETB gets enabled)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x3) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (both ITM and ETM go to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x1) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (only ETM goes to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (value == 0x2) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB enabled (only ITM goes to ETB)";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Kinetis: ETB not enabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis_EnableGPIOForETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var value;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var enabled;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; enabled = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0x40048038, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ReadRegister( SIM_SCGC5, &amp;amp;value);&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (1&amp;lt;&amp;lt;13)) == 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (1&amp;lt;&amp;lt;13);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enabling internal clock to Port E&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0x40048038, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // WriteRegister(SIM_SCGC5, value);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; enabled = 1;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = __readMemory32(0x40048004, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ReadRegister( SIM_SOPT2, &amp;amp;value);&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((value &amp;amp; (1&amp;lt;&amp;lt;12)) == 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; value |= (1&amp;lt;&amp;lt;12);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Debug trace clock select = Core/system clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(value, 0x40048004, "Memory");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // WriteRegister(SIM_SOPT2, value);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; enabled = 1;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; // ---- Enabling Trace Pin Function ----&lt;/P&gt;&lt;P&gt;&amp;nbsp; // Trace data and clock pins, high drive strength&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* TRACE CLK and TRACE D0*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D000, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR0,&amp;nbsp; 0x00000700);&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D010, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR4, 0x00000740);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ( __getTracePortSize() &amp;gt;= 2 )&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable TRACE D1*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D00C, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR3,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; } &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ( __getTracePortSize() == 4 )&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable TRACE D2, D3*/;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D008, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR2,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; __writeMemory32(0x00000540, 0x4004D004, "Memory");&amp;nbsp; // WriteRegister(PORTE_PCR1,&amp;nbsp; 0x00000740);&lt;/P&gt;&lt;P&gt;&amp;nbsp; } &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis_DisableGPIOForETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; // TODO: Reverse actions above (back to defaults)?&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// This is common routine to configure trace on Kinetis&lt;/P&gt;&lt;P&gt;// Kinetis has 2 trace sources (ITM/ETM) and 3 export options (ETM/ETB/SWO).&lt;/P&gt;&lt;P&gt;// The following cases are possible:&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Nothing&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to TPIU (with ITM)&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to ETB, ITM to SWO&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ETM to TPIU, ITM to ETB&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;KinetisConfigureTrace()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var modemask;&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var etbena;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; modemask = __getTraceProperty(2);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Get mask of selected modes&lt;/P&gt;&lt;P&gt;&amp;nbsp; etbena&amp;nbsp;&amp;nbsp; = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mask of bits for TPIU&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; if (modemask &amp;amp; 0x6) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ETB (0x4) or SWO (0x2) are allowed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (modemask &amp;amp; 0x2) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Only ETM should go to ETB &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x1 | 0x2;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Both ETM and ITM should go to ETB &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; etbena = 0x0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Both ETM and SWO go to TPIU&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; /*Check device for ETB*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; if( __readMemory32(0xE00FF018,"Memory") &amp;amp; 0x1)&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; Kinetis_EnableETB(etbena);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure what goes to ETB&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; if (modemask &amp;amp; 0x10) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Is ETM enabled?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_EnableGPIOForETM();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Yes - enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kinetis_calibrate != 3) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set calibration (only once time)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kinetis_calibrate = 3;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (__probeType("JTAGJet"))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __probeCmd("trace calibrate 3");&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // For Kinetis calibrate 3 works the best&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_DisableGPIOForETM();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;execConfigureTraceETM()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!__driverType("ijet")) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Compatible mode (other probes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis_EnableGPIOForETM(); // Enable GPIO for ETM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; // This native (ijet) driver (extended functionality)&lt;/P&gt;&lt;P&gt;&amp;nbsp; KinetisConfigureTrace();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Common configuration (for SWO and ETM)&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;execConfigureTraceSWO()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (!__driverType("ijet")) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Compatible mode (other probes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Nothing (as it was in original DMAC file).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; // This native (ijet) driver (extended functionality)&lt;/P&gt;&lt;P&gt;&amp;nbsp; KinetisConfigureTrace();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Common configuration (for SWO and ETM)&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MassErase()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; if (__hasDAPRegs())&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __var mdm_ctrl;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Select bank 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeDPReg(0x01000000, 0x8);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (__readAPReg(0x0) &amp;amp; 0x20)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mdm_ctrl = __readAPReg(0x4) | 0x1;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Do mass erase&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __writeAPReg(mdm_ctrl, 0x4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Performing mass erase...";&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Wait until finished&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; do&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __delay(100);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; } while(__readAPReg(0x4) &amp;amp; 0x1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase finished";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase is disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __message "Mass erase cannot be performed";&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;getPersistentQuickLaunchMacros()&amp;nbsp;&amp;nbsp; // &amp;lt;-- Reserved name, debugger calls it to populate QuickLaunch view.&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; __message "getPersistentQuickLaunchMacros";&lt;/P&gt;&lt;P&gt;&amp;nbsp; __var macs;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; macs = "MassErase()";&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; return macs;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 08:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-Keil-ETM-Tracing/m-p/238013#M5621</guid>
      <dc:creator>DaveTonyCook</dc:creator>
      <dc:date>2015-07-28T08:35:07Z</dc:date>
    </item>
  </channel>
</rss>