<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Enter, enable EZPORT via JTAG</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010317#M56083</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does EzPort work correct if you configure Flash Configuration Field?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you able to establish communication over EzPort (read the EzPort status register)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2020 23:42:43 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2020-03-13T23:42:43Z</dc:date>
    <item>
      <title>Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010316#M56082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using the MK64FX512.&lt;/P&gt;&lt;P&gt;I was successfull in entering both, JTAG and EZPORT with the right EZP.CS and reset start sequences.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem now is: i want to enable EZPORT not via RESET sequence, but via JTAG. If you look into the datasheet at the chapter JTAG Controller you find the EZPORT enable JTAG-instruction. But there is no description of this instruction.&lt;/P&gt;&lt;P&gt;I tried the following out:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- enter JTAG&lt;/P&gt;&lt;P&gt;- reset JTAG&lt;/P&gt;&lt;P&gt;- write 0xd to the instruction register&lt;/P&gt;&lt;P&gt;- enter run test/idle state&lt;/P&gt;&lt;P&gt;- try to reach EZPORT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found out, that after writing 0xd into the instruction register and entering idle, the chip itself stays at reset state (no pull-up an the reset pin asserted from the chip itself) until JTAG wasn't reset.&lt;/P&gt;&lt;P&gt;The program i programmed to the chip before has the EZPORT disabled in the flash configuration field. Is it possible to enable EZPORT although it is disabled in the flash config field? Maybe i must do an mass erase before trying to reach the EZPORT?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 11:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010316#M56082</guid>
      <dc:creator>schwimmen</dc:creator>
      <dc:date>2020-03-10T11:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010317#M56083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does EzPort work correct if you configure Flash Configuration Field?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you able to establish communication over EzPort (read the EzPort status register)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 23:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010317#M56083</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-03-13T23:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010318#M56084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felipe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the chip i try to reach via EZP is disabled via the flash configuration. At other chips i've changed the firmware, so EZP is enabled in the flash config. At these chips i have full access.&lt;/P&gt;&lt;P&gt;I know the chip i've tried is working, because i see the program running and i have connection via JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because i am new to JTAG, i don't know how do a mass erase over JTAG. It's hard to find any documentation, which is easy to read. All i know is, that i can reach flash using the ARM JTAG-DP. But how to use commands and select registers and stuff, i don't really now and it is hard to find out via the ARM documentary.&lt;A href="mailto:don@t"&gt;don@t&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried out to activate EZP via JTAG on a chip, where EZP is enabled in the flash config. There still is the same - the chip will stuck in the TAP or reset state after performing the JTAG-EZPORT command, until i reset the TAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2020 13:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010318#M56084</guid>
      <dc:creator>schwimmen</dc:creator>
      <dc:date>2020-03-14T13:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010319#M56085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, i've understood JTAG a bit, or better the interaction between the JTAG-DP and JTAG-AP. So now i was successfull in mass erasing the chip and therefore using EZPORT again on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But nevertheless it would be interesting to know the EZPORT enable command in the JTAG works. If it needs a certain time to start EZP, if there are any registers where you can see if the EZP was started successfully. In the manuals or application notes for the chip i am using, this command is not documented. Also i can't find in any other documents information about this command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Mar 2020 15:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010319#M56085</guid>
      <dc:creator>schwimmen</dc:creator>
      <dc:date>2020-03-15T15:25:52Z</dc:date>
    </item>
    <item>
      <title>Re: Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010320#M56086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is true that there is not enough information regarding this issue. I am going to ask this internally to see if there is any information I can provide. I will let you know as soon as I receive any update.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 21:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010320#M56086</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-03-19T21:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: Enter, enable EZPORT via JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010321#M56087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have received the following feedback from internal team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;It not possible to enable EZPORT although it is disabled in the flash config field.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for more information on EZPORT, please refer to&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102282"&gt;How to use EzPort module&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for noted that EZPORT is old programming interface, and further parts will not have it.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 19:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enter-enable-EZPORT-via-JTAG/m-p/1010321#M56087</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-03-20T19:47:50Z</dc:date>
    </item>
  </channel>
</rss>