<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Is there any code example of using FRDM KW41Z sensors?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-any-code-example-of-using-FRDM-KW41Z-sensors/m-p/1009610#M56068</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The project which I am working on has FreeRTOS on FRDM-KW41Z. I would like to know if there is an example of using board sensors within FreeRTOS?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2020 14:02:15 GMT</pubDate>
    <dc:creator>satsok_n</dc:creator>
    <dc:date>2020-01-28T14:02:15Z</dc:date>
    <item>
      <title>Is there any code example of using FRDM KW41Z sensors?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-any-code-example-of-using-FRDM-KW41Z-sensors/m-p/1009610#M56068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The project which I am working on has FreeRTOS on FRDM-KW41Z. I would like to know if there is an example of using board sensors within FreeRTOS?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 14:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-any-code-example-of-using-FRDM-KW41Z-sensors/m-p/1009610#M56068</guid>
      <dc:creator>satsok_n</dc:creator>
      <dc:date>2020-01-28T14:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any code example of using FRDM KW41Z sensors?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-any-code-example-of-using-FRDM-KW41Z-sensors/m-p/1009611#M56069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kostas, I hope you're doing well!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you're using connectivity Stack along with the sensors, I would recommend checking the BLE Temperature Sensor SDK example:&lt;/P&gt;&lt;P&gt;&amp;lt;…\SDK_SDK_2.2.1_FRDM-KW41Z\boards\frdmkw41z\wireless_examples\bluetooth\temperature_sensor\freertos&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This example uses the on-board Temperature Sensor to reports it to the Temperature Collector device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other useful examples are the FreeRTOS driver SDK Examples for I2C or SPI (depending on the type of sensor you'll be using).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These can be found in the following path:&lt;/P&gt;&lt;P&gt;&amp;lt;…\SDK_SDK_2.2.1_FRDM-KW41Z\boards\frdmkw41z\rtos_examples&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if you need any more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 17:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-any-code-example-of-using-FRDM-KW41Z-sensors/m-p/1009611#M56069</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-01-31T17:43:12Z</dc:date>
    </item>
  </channel>
</rss>