<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックAvailable pins for TRACE_CLKOUT on K64</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Available-pins-for-TRACE-CLKOUT-on-K64/m-p/1004240#M55983</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a K64F in MAPBGA 144 package and have a debug header wired to the MCU requiring routing of the TRACE_CLKOUT signal to pin D3. The K64 Sub-Family Data Sheet indicates in the Pinout chapter that pin D3 can be routed for TRACE_CLKOUT using the ALT5 mux configuration. By contrast, I noticed that in the MCUXpresso Config Tools &amp;gt; Pins view &amp;gt; Peripheral Signals tab, the SIM &amp;gt; CLKOUT signal only has two pins available to it: A11 and J7. This is in direct conflict with the K64 Sub-Family Data Sheet. Which information is accurate?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jan 2020 21:11:43 GMT</pubDate>
    <dc:creator>aberger</dc:creator>
    <dc:date>2020-01-13T21:11:43Z</dc:date>
    <item>
      <title>Available pins for TRACE_CLKOUT on K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Available-pins-for-TRACE-CLKOUT-on-K64/m-p/1004240#M55983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a K64F in MAPBGA 144 package and have a debug header wired to the MCU requiring routing of the TRACE_CLKOUT signal to pin D3. The K64 Sub-Family Data Sheet indicates in the Pinout chapter that pin D3 can be routed for TRACE_CLKOUT using the ALT5 mux configuration. By contrast, I noticed that in the MCUXpresso Config Tools &amp;gt; Pins view &amp;gt; Peripheral Signals tab, the SIM &amp;gt; CLKOUT signal only has two pins available to it: A11 and J7. This is in direct conflict with the K64 Sub-Family Data Sheet. Which information is accurate?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 21:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Available-pins-for-TRACE-CLKOUT-on-K64/m-p/1004240#M55983</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2020-01-13T21:11:43Z</dc:date>
    </item>
    <item>
      <title>Re: Available pins for TRACE_CLKOUT on K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Available-pins-for-TRACE-CLKOUT-on-K64/m-p/1004241#M55984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The D3 is not belong to the SIM. It belongs to TPIU. You will find D3 under the peripheral TPIU.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2020 01:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Available-pins-for-TRACE-CLKOUT-on-K64/m-p/1004241#M55984</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-01-14T01:58:40Z</dc:date>
    </item>
  </channel>
</rss>