<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K27F-K28F USB VREG_OUT Capacitor in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002817#M55946</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The capacitor is used to stabilise the low dropout regulator used to supply stable USB PHY power supply. This means that if FS USB is used it must be connected.&lt;SPAN style="text-decoration: underline;"&gt; If not, USB will not work.&lt;/SPAN&gt;&lt;BR /&gt;Make sure that the capacitor type used fulfills the low ESD requirements as specified in the manual and data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jan 2020 20:22:45 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-01-13T20:22:45Z</dc:date>
    <item>
      <title>K27F-K28F USB VREG_OUT Capacitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002816#M55945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just want to know if VREG_OUT (pin G2)&amp;nbsp;should be connected to an external output capacitor (COUT=2.2uF in datasheet) despite of it is not used to power any external circuit. I want to use USB FS with IRC48 as clock source. The microcontroller is powered by&amp;nbsp;an external supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 14:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002816#M55945</guid>
      <dc:creator>etronic_arg</dc:creator>
      <dc:date>2020-01-13T14:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: K27F-K28F USB VREG_OUT Capacitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002817#M55946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The capacitor is used to stabilise the low dropout regulator used to supply stable USB PHY power supply. This means that if FS USB is used it must be connected.&lt;SPAN style="text-decoration: underline;"&gt; If not, USB will not work.&lt;/SPAN&gt;&lt;BR /&gt;Make sure that the capacitor type used fulfills the low ESD requirements as specified in the manual and data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 20:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002817#M55946</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-01-13T20:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: K27F-K28F USB VREG_OUT Capacitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002818#M55947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. Just as I&amp;nbsp;thought! I&amp;nbsp;didn't realize to put it in my board...&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 21:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K27F-K28F-USB-VREG-OUT-Capacitor/m-p/1002818#M55947</guid>
      <dc:creator>etronic_arg</dc:creator>
      <dc:date>2020-01-13T21:39:05Z</dc:date>
    </item>
  </channel>
</rss>