<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: high-current drive MKE04Z128VLD4</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002505#M55932</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your teachings. It is said that Japanese is difficult to understand because the subject is ambiguous, but English has a similar situation. understood. PTH is not a 44-pin type. The understanding was shallow. Other than that, I was relieved to know that it was a 44-pin type.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Dec 2019 23:11:38 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2019-12-04T23:11:38Z</dc:date>
    <item>
      <title>high-current drive MKE04Z128VLD4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002503#M55930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for helping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. MKE04Z128VLD4 44pin is used.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; As you can see, does this package support high current output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. “8 PINOUT” in the MKE04P80M48SF0 manual stated “PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0, and PTH1 are high-current drive pins when operated as output.”&lt;BR /&gt;I thought I could use that function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. In the notes of `` 5.1.1 DC characteristics '', `` 2. Only PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0 (64-pin and 80-pin packages only), and PTH1 (64-pin and 80- pin packages only) support high current output. "&lt;BR /&gt;I found that description after creating the board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I think it ’s very unfriendly.&lt;/P&gt;&lt;P&gt;So far, complaints about confirmation and manual unkindness.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 09:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002503#M55930</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-12-03T09:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: high-current drive MKE04Z128VLD4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002504#M55931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;MKE04Z128VLD4 really has high current pin. PTB4, PTB5, PTD0, PTD1, PTE0, PTE1 still are high current pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"Only PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0 (64-pin and 80-pin packages only), and PTH1 (64-pin and 80- pin packages only) support high current output. "&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to say this sentence looks have problem. I'm sorry for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 07:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002504#M55931</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-12-04T07:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: high-current drive MKE04Z128VLD4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002505#M55932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your teachings. It is said that Japanese is difficult to understand because the subject is ambiguous, but English has a similar situation. understood. PTH is not a 44-pin type. The understanding was shallow. Other than that, I was relieved to know that it was a 44-pin type.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 23:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/high-current-drive-MKE04Z128VLD4/m-p/1002505#M55932</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-12-04T23:11:38Z</dc:date>
    </item>
  </channel>
</rss>