<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: full description of FRDM-K64F in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002274#M55916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have found register addresses in the document you provided. Many thanks!&lt;/P&gt;&lt;P&gt;Now I'm trying to execute my first assembler code with this board based on a version I have for another board and I got some errors:&lt;/P&gt;&lt;P&gt;1. There are some compilation errors. However, the .axf is generated. I guess the error is in the .c files, which it is supposed that I'm not using. I guess for this reason they are not critical. Am I ok? how can I remove this .c and .h files from the target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;Rebuild started: Project: FRDMexample&lt;/EM&gt;
&lt;EM&gt;*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'&lt;/EM&gt;
&lt;EM&gt;Rebuild target 'Target 1'&lt;/EM&gt;
&lt;EM&gt;assembling FRDMexample.s...&lt;/EM&gt;
&lt;EM&gt;assembling startup_MK64F12.s...&lt;/EM&gt;
&lt;EM&gt;compiling system_MK64F12.c...&lt;/EM&gt;
&lt;EM&gt;compiling startup.c...&lt;/EM&gt;
&lt;EM&gt;C:\Users\faundez\AppData\Local\Arm\Packs\Keil\Kinetis_SDK_DFP\2.3.0\platform\devices\startup.c(68): warning:&amp;nbsp; #47-D: incompatible redefinition of macro "__VECTOR_TABLE"&amp;nbsp; (declared at line 126 of "C:\Users\faundez\AppData\Local\Arm\Packs\ARM\CMSIS\5.6.0\CMSIS\Core\Include\cmsis_armcc.h")&lt;/EM&gt;
&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define __VECTOR_TABLE Image$$VECTOR_ROM$$Base&amp;nbsp; &lt;/EM&gt;
&lt;EM&gt;C:\Users\faundez\AppData\Local\Arm\Packs\Keil\Kinetis_SDK_DFP\2.3.0\platform\devices\startup.c: 1 warning, 0 errors&lt;/EM&gt;
&lt;EM&gt;linking...&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6914W: option ro-base ignored when using --scatter.&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6914W: option rw-base ignored when using --scatter.&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6340W: options first and last are ignored for link type of scattered&lt;/EM&gt;
&lt;EM&gt;./RTE/Device/MK64FN1M0VLL12/MK64FN1M0xxx12_flash.scf(90): warning: L6314W: No section matches pattern *(InRoot$$Sections).&lt;/EM&gt;
&lt;EM&gt;Program Size: Code=380 RO-data=1040 RW-data=0 ZI-data=2048&amp;nbsp; &lt;/EM&gt;
&lt;EM&gt;Finished: 0 information, 4 warning and 0 error messages.&lt;/EM&gt;
&lt;EM&gt;".\Objects\FRDMexample.axf" - 0 Error(s), 5 Warning(s).&lt;/EM&gt;
&lt;EM&gt;Build Time Elapsed:&amp;nbsp; 00:00:06&lt;/EM&gt;
&lt;EM&gt;Load "C:\\Keil\\ejemplo\\Objects\\FRDMexample.axf" &lt;/EM&gt;
&lt;EM&gt;Internal DLL Error&lt;/EM&gt;
&lt;EM&gt;Error: Flash Download failed&amp;nbsp; -&amp;nbsp; Target DLL has been cancelled&lt;/EM&gt;
&lt;EM&gt;Flash Load finished at 00:14:40&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. When I try to load the code in the FRDMK64 board I got the following error: no ulink2/ME device. I think this is because I have not setup the proper debug. According to Keil it seems that this board uses JTAG/SW (&lt;A class="link-titled" href="http://www.keil.com/boards2/nxp/frdm_k64f/" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank" title="http://www.keil.com/boards2/nxp/frdm_k64f/"&gt;MDK5 - NXP FRDM-K64F&lt;/A&gt;&amp;nbsp; ). However, I do not see this option available in keil 5.29. How should I fix that? Please, consider that this is my first time trying to work with this development board. My previous experience is with launchpad TIVA TM4C123 mainly in C&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="FRDM.png"&gt;&lt;IMG alt="FRDM.png" src="https://community.nxp.com/t5/image/serverpage/image-id/95932i8CEBE30733D60291/image-size/large?v=v2&amp;amp;px=999" title="FRDM.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This is my assembler code, based on a document "GPIO example in Kinetis design studio (KDS) with FRDM-K64F" by Paul Garate &amp;amp; Augusto Panecatl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt;; Assembler example&lt;BR /&gt;; SW2 press -&amp;gt; green color&lt;BR /&gt;; SW3 press -&amp;gt; blue color&lt;BR /&gt;; SW2 and SW3 pressed -&amp;gt; red color&lt;/DIV&gt;&lt;DIV&gt;SIM_SCGC5 EQU 0x40048038&amp;nbsp;;clock activation&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;PORTB_PCR21 EQU 0x4004A054;Blue led&lt;BR /&gt;PORTB_PCR22 EQU 0x4004A058;Red led&lt;BR /&gt;PORTE_PCR26 EQU 0x4004D068;Green led&lt;BR /&gt;PORTC_PCR6 EQU 0x4004B018; switch 2&lt;BR /&gt;PORTA_PCR4 EQU 0x40049010; swith 3&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;GPIOA_PDDR EQU 0x400FF014; Port A Data Direction Register&lt;BR /&gt;GPIOB_PDDR EQU 0x400FF054; Port B Data Direction Register&lt;BR /&gt;GPIOC_PDDR EQU 0x400FF094; Port C Data Direction Register&lt;BR /&gt;GPIOE_PDDR EQU 0x400FF114; Port E Data Direction Register&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;GPIOC_PDIR EQU 0x400FF090; Port C Data Input Register&lt;BR /&gt;GPIOA_PDIR EQU 0x400FF010; Port A Data Input Register&lt;/DIV&gt;&lt;DIV&gt;GPIOB_PDOR EQU 0x400FF040; Port B Data Output Register&lt;BR /&gt;GPIOE_PDOR EQU 0x400FF100; Port E Data Output Register&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;SEC_DIV_FIVE EQU 1066666 ; 1 second divided by 5&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;AREA |.text|,CODE,READONLY, ALIGN=2&lt;BR /&gt;&amp;nbsp;THUMB&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;EXPORT __main&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;__main&lt;BR /&gt;&amp;nbsp;BL GPIO_Init&lt;BR /&gt;Loop&amp;nbsp; &lt;BR /&gt;&amp;nbsp;LDR R0,=SEC_DIV_FIVE&lt;BR /&gt;&amp;nbsp;BL delay&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOC_PDIR&lt;BR /&gt;&amp;nbsp;LDR R0,[R1]&lt;BR /&gt;&amp;nbsp;CMP R0,#0x00&amp;nbsp;;Switch 2 was pressed&lt;BR /&gt;&amp;nbsp;BEQ SWITCH2_ON&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOA_PDIR&lt;BR /&gt;&amp;nbsp;LDR R0,[R1]&lt;BR /&gt;&amp;nbsp;CMP R0,#0x00&amp;nbsp;;Switch 3 was pressed&lt;BR /&gt;&amp;nbsp;BEQ SWITCH3_ON&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;B Loop&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;SWITCH2_ON ;turn on green&lt;BR /&gt;&amp;nbsp;MOV R0,#0x04000000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOE_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;SWITCH3_ON ;turn on blue&lt;BR /&gt;&amp;nbsp;MOV R0,#0x00400000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOB_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;/DIV&gt;&lt;DIV&gt;BOTH_SWITCHES ;turn on red&lt;BR /&gt;&amp;nbsp;MOV R0,#0x00200000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOB_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;BR /&gt;delay&lt;BR /&gt;&amp;nbsp;SUBS R0,R0,#1&lt;BR /&gt;&amp;nbsp;BNE delay&lt;BR /&gt;&amp;nbsp;BX LR&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;GPIO_Init&lt;BR /&gt;&amp;nbsp; LDR R1,=SIM_SCGC5&lt;BR /&gt;&amp;nbsp; LDR R0,[R1]&lt;BR /&gt;&amp;nbsp; ORR R0,R0,#0x2700&amp;nbsp;;Port A, B, C, E&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; LDR R1,=PORTB_PCR21&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTB_PCR22&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTE_PCR26&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTC_PCR6&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTA_PCR4&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOA_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x0010&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOB_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x00600000&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOC_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x00000040&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOE_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x04000000&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; BX LR&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; ALIGN&lt;BR /&gt;&amp;nbsp; END&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Nov 2020 14:33:14 GMT</pubDate>
    <dc:creator>faundez</dc:creator>
    <dc:date>2020-11-02T14:33:14Z</dc:date>
    <item>
      <title>full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002271#M55913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, so far I have been using Texas launchpad TIVA with Keil and now I want to try the development board FRDM-K64F. I have the board but I was unable to find a document with the full description of registers (addresses, configuration etc.)&lt;/P&gt;&lt;P&gt;I have been looking in this link:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/freedom-development-platform-for-kinetis-k64-k63-and-k24-mcus:FRDM-K64F" title="https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/freedom-development-platform-for-kinetis-k64-k63-and-k24-mcus:FRDM-K64F"&gt;FRDM-K64F Platform|Freedom Development Board|Kinetis MCUs | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and I'm looking for something fully complete like this one&amp;nbsp;&lt;A class="link-titled" href="http://www.ti.com/lit/ds/spms376e/spms376e.pdf" title="http://www.ti.com/lit/ds/spms376e/spms376e.pdf"&gt;http://www.ti.com/lit/ds/spms376e/spms376e.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some info/ examples using Keil uVision Will also be appreciated&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Marcos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 12:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002271#M55913</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-03T12:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002272#M55914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Registers are described in the users manual: &lt;A class="link-titled" href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/k-series-cortex-m4/k6x-ethernet/kinetis-k64-120-mhz-256-kb-sram-microcontrollers-mcus-based-on-arm-cortex-m4-core:K64_120?tab=Documentation_Tab" title="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/k-series-cortex-m4/k6x-ethernet/kinetis-k64-120-mhz-256-kb-sram-microcontrollers-mcus-based-on-arm-cortex-m4-core:K64_120?tab=Documentation_Tab"&gt;Arm® Cortex®-M4|Kinetis® K64 120 MHz 32-bit MCUs | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Complete Kinetis solutions for faster/more efficient professional needs, training and support: &lt;A href="http://www.utasker.com/kinetis.html" target="test_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i.MX RT project compatibility: &lt;A href="http://www.utasker.com/iMX.html" target="test_blank"&gt;http://www.utasker.com/iMX.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Including FreeRTOS integration for all Kinetis parts&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Kinetis K64:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/FRDM-K64F.html" target="test_blank"&gt;http://www.utasker.com/kinetis/FRDM-K64F.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/TWR-K64F120M.html" target="test_blank"&gt;http://www.utasker.com/kinetis/TWR-K64F120M.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/TEENSY_3.5.html" target="test_blank"&gt;http://www.utasker.com/kinetis/TEENSY_3.5.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/Hexiwear-K64F.html" target="test_blank"&gt;http://www.utasker.com/kinetis/Hexiwear-K64F.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN style="color: #000080;"&gt;&lt;EM&gt;uTasker: supporting &amp;gt;1'000 registered Kinetis users get products faster and cheaper to market&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Request Free emergency remote desk-top consulting at &lt;A href="http://www.utasker.com/services.html" target="test_blank"&gt;http://www.utasker.com/services.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Open Source version at &lt;A href="https://github.com/uTasker/uTasker-Kinetis" target="test_blank"&gt;https://github.com/uTasker/uTasker-Kinetis&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;A href="https://community.nxp.com/thread/512558" target="test_blank"&gt;https://community.nxp.com/thread/512558&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;A href="https://community.nxp.com/thread/352862" target="test_blank"&gt;https://community.nxp.com/thread/352862&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;A href="https://community.nxp.com/thread/498809" target="test_blank"&gt;https://community.nxp.com/thread/498809&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 21:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002272#M55914</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-12-03T21:40:01Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002273#M55915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="352389" data-username="faundez@tecnocampus.cat" href="https://community.nxp.com/people/faundez@tecnocampus.cat"&gt;Marcos Faundez Zanuy&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; K64 register document is the reference manual:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=K64P144M120SF5RM" title="https://www.nxp.com/webapp/Download?colCode=K64P144M120SF5RM"&gt;https://www.nxp.com/webapp/Download?colCode=K64P144M120SF5RM&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 06:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002273#M55915</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-12-04T06:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002274#M55916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have found register addresses in the document you provided. Many thanks!&lt;/P&gt;&lt;P&gt;Now I'm trying to execute my first assembler code with this board based on a version I have for another board and I got some errors:&lt;/P&gt;&lt;P&gt;1. There are some compilation errors. However, the .axf is generated. I guess the error is in the .c files, which it is supposed that I'm not using. I guess for this reason they are not critical. Am I ok? how can I remove this .c and .h files from the target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;Rebuild started: Project: FRDMexample&lt;/EM&gt;
&lt;EM&gt;*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'&lt;/EM&gt;
&lt;EM&gt;Rebuild target 'Target 1'&lt;/EM&gt;
&lt;EM&gt;assembling FRDMexample.s...&lt;/EM&gt;
&lt;EM&gt;assembling startup_MK64F12.s...&lt;/EM&gt;
&lt;EM&gt;compiling system_MK64F12.c...&lt;/EM&gt;
&lt;EM&gt;compiling startup.c...&lt;/EM&gt;
&lt;EM&gt;C:\Users\faundez\AppData\Local\Arm\Packs\Keil\Kinetis_SDK_DFP\2.3.0\platform\devices\startup.c(68): warning:&amp;nbsp; #47-D: incompatible redefinition of macro "__VECTOR_TABLE"&amp;nbsp; (declared at line 126 of "C:\Users\faundez\AppData\Local\Arm\Packs\ARM\CMSIS\5.6.0\CMSIS\Core\Include\cmsis_armcc.h")&lt;/EM&gt;
&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define __VECTOR_TABLE Image$$VECTOR_ROM$$Base&amp;nbsp; &lt;/EM&gt;
&lt;EM&gt;C:\Users\faundez\AppData\Local\Arm\Packs\Keil\Kinetis_SDK_DFP\2.3.0\platform\devices\startup.c: 1 warning, 0 errors&lt;/EM&gt;
&lt;EM&gt;linking...&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6914W: option ro-base ignored when using --scatter.&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6914W: option rw-base ignored when using --scatter.&lt;/EM&gt;
&lt;EM&gt;.\Objects\FRDMexample.axf: Warning: L6340W: options first and last are ignored for link type of scattered&lt;/EM&gt;
&lt;EM&gt;./RTE/Device/MK64FN1M0VLL12/MK64FN1M0xxx12_flash.scf(90): warning: L6314W: No section matches pattern *(InRoot$$Sections).&lt;/EM&gt;
&lt;EM&gt;Program Size: Code=380 RO-data=1040 RW-data=0 ZI-data=2048&amp;nbsp; &lt;/EM&gt;
&lt;EM&gt;Finished: 0 information, 4 warning and 0 error messages.&lt;/EM&gt;
&lt;EM&gt;".\Objects\FRDMexample.axf" - 0 Error(s), 5 Warning(s).&lt;/EM&gt;
&lt;EM&gt;Build Time Elapsed:&amp;nbsp; 00:00:06&lt;/EM&gt;
&lt;EM&gt;Load "C:\\Keil\\ejemplo\\Objects\\FRDMexample.axf" &lt;/EM&gt;
&lt;EM&gt;Internal DLL Error&lt;/EM&gt;
&lt;EM&gt;Error: Flash Download failed&amp;nbsp; -&amp;nbsp; Target DLL has been cancelled&lt;/EM&gt;
&lt;EM&gt;Flash Load finished at 00:14:40&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. When I try to load the code in the FRDMK64 board I got the following error: no ulink2/ME device. I think this is because I have not setup the proper debug. According to Keil it seems that this board uses JTAG/SW (&lt;A class="link-titled" href="http://www.keil.com/boards2/nxp/frdm_k64f/" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank" title="http://www.keil.com/boards2/nxp/frdm_k64f/"&gt;MDK5 - NXP FRDM-K64F&lt;/A&gt;&amp;nbsp; ). However, I do not see this option available in keil 5.29. How should I fix that? Please, consider that this is my first time trying to work with this development board. My previous experience is with launchpad TIVA TM4C123 mainly in C&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="FRDM.png"&gt;&lt;IMG alt="FRDM.png" src="https://community.nxp.com/t5/image/serverpage/image-id/95932i8CEBE30733D60291/image-size/large?v=v2&amp;amp;px=999" title="FRDM.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This is my assembler code, based on a document "GPIO example in Kinetis design studio (KDS) with FRDM-K64F" by Paul Garate &amp;amp; Augusto Panecatl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt;; Assembler example&lt;BR /&gt;; SW2 press -&amp;gt; green color&lt;BR /&gt;; SW3 press -&amp;gt; blue color&lt;BR /&gt;; SW2 and SW3 pressed -&amp;gt; red color&lt;/DIV&gt;&lt;DIV&gt;SIM_SCGC5 EQU 0x40048038&amp;nbsp;;clock activation&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;PORTB_PCR21 EQU 0x4004A054;Blue led&lt;BR /&gt;PORTB_PCR22 EQU 0x4004A058;Red led&lt;BR /&gt;PORTE_PCR26 EQU 0x4004D068;Green led&lt;BR /&gt;PORTC_PCR6 EQU 0x4004B018; switch 2&lt;BR /&gt;PORTA_PCR4 EQU 0x40049010; swith 3&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;GPIOA_PDDR EQU 0x400FF014; Port A Data Direction Register&lt;BR /&gt;GPIOB_PDDR EQU 0x400FF054; Port B Data Direction Register&lt;BR /&gt;GPIOC_PDDR EQU 0x400FF094; Port C Data Direction Register&lt;BR /&gt;GPIOE_PDDR EQU 0x400FF114; Port E Data Direction Register&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;GPIOC_PDIR EQU 0x400FF090; Port C Data Input Register&lt;BR /&gt;GPIOA_PDIR EQU 0x400FF010; Port A Data Input Register&lt;/DIV&gt;&lt;DIV&gt;GPIOB_PDOR EQU 0x400FF040; Port B Data Output Register&lt;BR /&gt;GPIOE_PDOR EQU 0x400FF100; Port E Data Output Register&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;SEC_DIV_FIVE EQU 1066666 ; 1 second divided by 5&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;AREA |.text|,CODE,READONLY, ALIGN=2&lt;BR /&gt;&amp;nbsp;THUMB&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;EXPORT __main&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;__main&lt;BR /&gt;&amp;nbsp;BL GPIO_Init&lt;BR /&gt;Loop&amp;nbsp; &lt;BR /&gt;&amp;nbsp;LDR R0,=SEC_DIV_FIVE&lt;BR /&gt;&amp;nbsp;BL delay&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOC_PDIR&lt;BR /&gt;&amp;nbsp;LDR R0,[R1]&lt;BR /&gt;&amp;nbsp;CMP R0,#0x00&amp;nbsp;;Switch 2 was pressed&lt;BR /&gt;&amp;nbsp;BEQ SWITCH2_ON&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOA_PDIR&lt;BR /&gt;&amp;nbsp;LDR R0,[R1]&lt;BR /&gt;&amp;nbsp;CMP R0,#0x00&amp;nbsp;;Switch 3 was pressed&lt;BR /&gt;&amp;nbsp;BEQ SWITCH3_ON&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;B Loop&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;SWITCH2_ON ;turn on green&lt;BR /&gt;&amp;nbsp;MOV R0,#0x04000000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOE_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;SWITCH3_ON ;turn on blue&lt;BR /&gt;&amp;nbsp;MOV R0,#0x00400000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOB_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;/DIV&gt;&lt;DIV&gt;BOTH_SWITCHES ;turn on red&lt;BR /&gt;&amp;nbsp;MOV R0,#0x00200000&lt;BR /&gt;&amp;nbsp;LDR R1,=GPIOB_PDOR&lt;BR /&gt;&amp;nbsp;STR R0,[R1]&lt;BR /&gt;&amp;nbsp;B Loop&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;BR /&gt;delay&lt;BR /&gt;&amp;nbsp;SUBS R0,R0,#1&lt;BR /&gt;&amp;nbsp;BNE delay&lt;BR /&gt;&amp;nbsp;BX LR&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;GPIO_Init&lt;BR /&gt;&amp;nbsp; LDR R1,=SIM_SCGC5&lt;BR /&gt;&amp;nbsp; LDR R0,[R1]&lt;BR /&gt;&amp;nbsp; ORR R0,R0,#0x2700&amp;nbsp;;Port A, B, C, E&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; LDR R1,=PORTB_PCR21&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTB_PCR22&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTE_PCR26&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTC_PCR6&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=PORTA_PCR4&lt;BR /&gt;&amp;nbsp; MOV R0,#0x100&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOA_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x0010&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOB_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x00600000&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOC_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x00000040&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; LDR R1,=GPIOE_PDDR&lt;BR /&gt;&amp;nbsp; MOV R0,#0x04000000&lt;BR /&gt;&amp;nbsp; STR R0,[R1]&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; BX LR&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; ALIGN&lt;BR /&gt;&amp;nbsp; END&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002274#M55916</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2020-11-02T14:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002275#M55917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="352389" data-username="faundez@tecnocampus.cat" href="https://community.nxp.com/people/faundez@tecnocampus.cat"&gt;Marcos Faundez Zanuy&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; About the K64 code, I highly recommend you use the official SDK code, that code already be tested, it contains the MDK project, please download the code from this link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Select the board as FRDM-K64, then generate the code and download it.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You will find the package already contains the doc and code folder, you can refer to the document in the doc at first to get start.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 03:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002275#M55917</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-12-09T03:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002276#M55918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if the doc is this one in cursive letters&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hardware requirements&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;=====================&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- Mini USB cable&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- FRDM-K64F board&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- Personal Computer&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Board settings&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;==============&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;This example project does not call for any special hardware configurations.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Although not required, the recommendation is to leave the development board's jumper settings&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;and configurations in default state when running this example.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Prepare the Demo&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;================&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1. Connect a USB cable between the PC host and the Debug Link port on the board.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2. Download the program to the target board.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Running the demo&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;================&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The log below shows the output of the led control demo in the terminal window:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The demo is used to demonstrate how to use new components.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The main function of the demo is to control the led by using the shell or button.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;For shell, please enter "help" to get the help information firstly. Turn on LED by using command "led on". And turn off LED by using command "led off".&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;For button, please press the button SW3 to control LED. Turn on LED when the button is pressed with long press or double click event. And turn off LED when the button is pressed with short press or one click event.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;SHELL build: Aug 30 2018&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Copyright 2018 NXP&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;led_control@SHELL&amp;gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I still miss the configuration for debugging. Which option should I select?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96006iC6AA4F04C7DF0494/image-size/large?v=v2&amp;amp;px=999" title="keil5.jpg" alt="keil5.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact when I try to upload it says &lt;STRONG&gt;no debug unit device found&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 10:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002276#M55918</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-09T10:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002277#M55919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you plug the FRDM-K64F into your PC it will show up as an external hard-drive and there you can see which debugger/loader is installed (it could be CMSIS-DAP, Jlink or PEMicro). Select this and then go into the debugger setting and set details, such as SWD mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get complete ready-to-build uVision projects for FRDM-K64F at the uTasker open source GIT hub link (USB, Ethernet, SD card, etc.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 21:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002277#M55919</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-12-09T21:45:58Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002278#M55920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Mark&lt;/P&gt;&lt;P&gt;yes, I see this disk&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96054i92D87AF062D4A647/image-size/large?v=v2&amp;amp;px=999" title="disk.jpg" alt="disk.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then I follow the web link, which brings to this page&amp;nbsp;&lt;A class="link-titled" href="https://www.segger.com/products/debug-probes/j-link/models/j-link-ob/" title="https://www.segger.com/products/debug-probes/j-link/models/j-link-ob/"&gt;https://www.segger.com/products/debug-probes/j-link/models/j-link-ob/&lt;/A&gt;&amp;nbsp;&amp;nbsp;where I check that the debugger is j-link.&lt;/P&gt;&lt;P&gt;then I set this debugger:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96055i065F8EB2723080BD/image-size/large?v=v2&amp;amp;px=999" title="set_debugger.jpg" alt="set_debugger.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I accept the terms&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96056iC557F7AA007802A5/image-size/large?v=v2&amp;amp;px=999" title="terms.jpg" alt="terms.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and I get this error&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96057iB14D2CE674202B40/image-size/large?v=v2&amp;amp;px=999" title="error.jpg" alt="error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;in the build line I can read&lt;/P&gt;&lt;P&gt;&lt;EM&gt;JLink info:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;------------&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DLL: V6.10i, compiled Oct 25 2016 19:31:51&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Firmware: J-Link OpenSDA 2 compiled Oct 13 2015 12:10:27&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Hardware: V1.00&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;S/N : 621000000 &lt;/EM&gt;&lt;BR /&gt; &lt;BR /&gt;&lt;EM&gt;***JLink Error: Debugger tries to select target interface JTAG.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;This interface is not supported by the connected emulator.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Selection will be ignored by the DLL.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: Flash Download failed - Target DLL has been cancelled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flash Load finished at 23:29:23&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I don't know how to fix that. Note that I don't have any additional hardware for debugging. Just the freescale development kit. I'm trying to execute the suggested example available in NXP website&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Marcos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PD: in case it helps: I installed again the packs for K6x but I got the same result&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96058i78B4A5AEB329C284/image-size/large?v=v2&amp;amp;px=999" title="comport.jpg" alt="comport.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 22:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002278#M55920</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-09T22:27:35Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002279#M55921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96059iD1D52DFF1CDEE220/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It says why it doesn't work - you still need to configure the debugger in the Segger JLInk setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a general ergonomics nightmare in uVision: It has to in fact be set up twice in two locations....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 00:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002279#M55921</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-12-10T00:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002280#M55922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, many thanks, I Will try this&amp;nbsp; &lt;A class="link-titled" href="https://www.segger.com/products/debug-probes/j-link/technology/ides/keil-mdk/" title="https://www.segger.com/products/debug-probes/j-link/technology/ides/keil-mdk/"&gt;https://www.segger.com/products/debug-probes/j-link/technology/ides/keil-mdk/&lt;/A&gt; &amp;nbsp;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;this afternoon&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;however, this is NOT a general keil problem. With Texas launchpad tiva is by far much more simple. It's a problem with this debugger.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 10:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002280#M55922</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-10T10:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002281#M55923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I modified the Port configuration and it tries&amp;nbsp; to load the code&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96158iEEC45AFB33DB0BF2/image-size/large?v=v2&amp;amp;px=999" title="targetsetup.jpg" alt="targetsetup.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;but it fails during verification&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96163i2468246DF63A1A2C/image-size/large?v=v2&amp;amp;px=999" title="keil5b.jpg" alt="keil5b.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;JLink info:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;------------&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DLL: V6.10i, compiled Oct 25 2016 19:31:51&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Firmware: J-Link OpenSDA 2 compiled Oct 13 2015 12:10:27&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Hardware: V1.00&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;S/N : 621000000 &lt;/EM&gt;&lt;BR /&gt; &lt;BR /&gt;&lt;EM&gt;* JLink Info: Found SWD-DP with ID 0x2BA01477&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: Found SWD-DP with ID 0x2BA01477&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: AP-IDR: 0x24770011, Type: AHB-AP&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: Found Cortex-M4 r0p1, Little endian.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: FPUnit: 6 code (BP) slots and 2 literal slots&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: CoreSight components:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 @ E00FF000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB00C SCS&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [3]: FFF01000, CID: B105E00D, PID: 003BB001 ITM&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [4]: FFF41000, CID: B105900D, PID: 000BB9A1 TPIU&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [5]: FFF42000, CID: B105900D, PID: 000BB925 ETM&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [6]: FFF43000, CID: B105900D, PID: 003BB907 ETB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* JLink Info: ROMTbl 0 [7]: FFF44000, CID: B105900D, PID: 001BB908 CSTF&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ROMTableAddr = 0xE00FF000&lt;/EM&gt;&lt;BR /&gt; &lt;BR /&gt;&lt;EM&gt;Target info:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;------------&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Device: MK64FN1M0xxx12&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VTarget = 3.300V&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;State of Pins: &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TCK: 0, TDI: 0, TDO: 0, TMS: 0, TRES: 0, TRST: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Hardware-Breakpoints: 6&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Software-Breakpoints: 8192&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Watchpoints: 4&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;JTAG speed: 1429 kHz&lt;/EM&gt;&lt;BR /&gt; &lt;BR /&gt;&lt;EM&gt;Erase Done.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Programming Done.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001CH (Flash=00H Required=96H) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001DH (Flash=00H Required=E6H) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001EH (Flash=00H Required=FCH) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001FH (Flash=00H Required=DFH) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Verify Failed!&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: Flash Download failed - "Cortex-M4"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flash Load finished at 16:07:57&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 15:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002281#M55923</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-10T15:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002282#M55924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="352389" data-username="faundez@tecnocampus.cat" href="https://community.nxp.com/people/faundez@tecnocampus.cat"&gt;Marcos Faundez Zanuy&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Click flashdownload item :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96329iA0D21E22343F76AF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Do you add the flash download algorithm?&lt;/P&gt;&lt;P&gt;I still suggest you try the official SDK MDK project directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 03:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002282#M55924</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-12-11T03:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002283#M55925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Kerry&lt;/P&gt;&lt;P&gt;I see this screen&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96532iBD68E2B9E35F2FF9/image-size/large?v=v2&amp;amp;px=999" title="flash_download.jpg" alt="flash_download.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and yes, I'm using the example provided by NXP &lt;EM&gt;led_control_bm&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;in my jlink disk (the freescale board) there is a text file that says&amp;nbsp;&lt;EM&gt;No valid VMSD configuration for target flashing found&lt;/EM&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;but I don't know how to fix that (where should I get this file?) NXP example consists of more than 200 files just to play with leds and switches!!!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96533iA9077789AB66351C/image-size/large?v=v2&amp;amp;px=999" title="folders.jpg" alt="folders.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Marcos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 20:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002283#M55925</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-11T20:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002284#M55926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI, I just uploaded the file&amp;nbsp;&lt;EM&gt;&lt;A href="https://www.segger.com/downloads/jlink/OpenSDA_FRDM-K64F" style="color: var(--google-blue-600); background-color: #ffffff; font-weight: 500; text-decoration: none;" tabindex="0"&gt;02_OpenSDA_FRDM-K64F.bin&lt;/A&gt;&lt;/EM&gt;&amp;nbsp;, which was downloaded from &lt;A class="link-titled" href="https://www.segger.com/downloads/jlink/#JLinkOpenSDABoardSpecificFirmwares" title="https://www.segger.com/downloads/jlink/#JLinkOpenSDABoardSpecificFirmwares"&gt;https://www.segger.com/downloads/jlink/#JLinkOpenSDABoardSpecificFirmwares&lt;/A&gt;&amp;nbsp; and pasted in the bootloader disk and now the flashinfo.txt says&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;This J-Link VMSD config can be used to flash a NXP MK64FN1M0xxx12 target device.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;however, I get the same error when trying to upload the code :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Programming Done.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001CH (Flash=00H Required=96H) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001DH (Flash=00H Required=E6H) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001EH (Flash=00H Required=FCH) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Contents mismatch at: 0000001FH (Flash=00H Required=DFH) !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Verify Failed!&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: Flash Download failed - "Cortex-M4"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flash Load finished at 00:26:44&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 23:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002284#M55926</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-11T23:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002285#M55927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="352389" data-username="faundez@tecnocampus.cat" href="https://community.nxp.com/people/faundez@tecnocampus.cat" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Marcos Faundez Zanuy&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;1. Please use the SDK_FRDM-K64 code is downloaded from this link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Select development board, choose the board as FRDM-K64, then open the SDK folder:&lt;/P&gt;&lt;P&gt;SDK_2.5.0_FRDM-K64F\boards\frdmk64f\demo_apps\led_blinky\mdk&lt;/P&gt;&lt;P&gt;Test led_blinky project.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You also can check&amp;nbsp;Getting Started with MCUXpresso SDK.pdf under:SDK_2.5.0_FRDM-K64F\docs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. You can also try the CMSIS DAP debugger&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F" title="https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F"&gt;OpenSDA Serial and Debug Adapter | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please help you to check what's the PC system you are using? If you are using the win10, you may also need to use the external debugger to update your FRDM-K64 onboard K20 bootloader firmware.&lt;/P&gt;&lt;P&gt;&amp;nbsp; More details, please check the above opensda link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I find your test project seems not from the SDK directly, so please download the newest SDK project, check your PC system, and the opensda, also test the CMSIS DAP debugger firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any updated information, please let me know.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 05:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002285#M55927</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-12-12T05:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002286#M55928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;even worse. Now I only see the bootloader and after copying the opensda and re-pluging again the board, windows does not detect the board. By the way, I use win'7.&lt;/P&gt;&lt;P&gt;I gave up keil uVision for this board. it is by far much more complex than launchpad TIVA. I will try now with MCUXpresso tools&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Marcos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 10:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002286#M55928</guid>
      <dc:creator>faundez</dc:creator>
      <dc:date>2019-12-12T10:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: full description of FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002287#M55929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="352389" data-username="faundez@tecnocampus.cat" href="https://community.nxp.com/people/faundez@tecnocampus.cat"&gt;Marcos Faundez Zanuy&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you modify the K20 chip code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; When you see the bootloader, which firmware you copy to the BOOTLOADER disc?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you have any external debugger, eg, JLINK, you can try to download the opensda2.2 firmware to the K20, then use the new &lt;SPAN class=""&gt;DAPLink rev0244 OpenSDA v2.2 Bootloade&lt;/SPAN&gt;r.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Of course, you also can try the MCUXpresso IDE, whether you can download the code or not with the JLINK firmware? Just to check whether your problem is in the debugger side or the IDE side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any updated information, please let me know.&lt;/P&gt;&lt;P&gt;Kerry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 02:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/full-description-of-FRDM-K64F/m-p/1002287#M55929</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-12-13T02:46:20Z</dc:date>
    </item>
  </channel>
</rss>