<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUsing Kinetis SPI without SIN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999558#M55857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a SPI port to write data to just an OLED display,&amp;nbsp;there is no SPI data output that I would connect to the SPI SIN - currently I'm tying the pin to VSS.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the obvious question is, could I use the pin I've allocated for SIN as a DI/DO and ignore what happens inside the chip?&amp;nbsp; Reading the RM, I don't see how this could be a problem, but I thought I'd ask the wise people here.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2019 22:08:43 GMT</pubDate>
    <dc:creator>myke_predko</dc:creator>
    <dc:date>2019-12-18T22:08:43Z</dc:date>
    <item>
      <title>Using Kinetis SPI without SIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999558#M55857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a SPI port to write data to just an OLED display,&amp;nbsp;there is no SPI data output that I would connect to the SPI SIN - currently I'm tying the pin to VSS.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the obvious question is, could I use the pin I've allocated for SIN as a DI/DO and ignore what happens inside the chip?&amp;nbsp; Reading the RM, I don't see how this could be a problem, but I thought I'd ask the wise people here.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 22:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999558#M55857</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2019-12-18T22:08:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using Kinetis SPI without SIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999559#M55858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If the SIN do not influence the communication between the master and slave, you can ignore it. And use it as general IO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------- &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 01:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999559#M55858</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2019-12-19T01:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: Using Kinetis SPI without SIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999560#M55859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you - it's nice getting the extra pin.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 01:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Kinetis-SPI-without-SIN/m-p/999560#M55859</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2019-12-19T01:54:30Z</dc:date>
    </item>
  </channel>
</rss>