<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KW36A BUCK AUTOSTART in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW36A-BUCK-AUTOSTART/m-p/996733#M55818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use KW36A chip in buck auto start mode. I have the VDCDCIN and DCDC-CFG and PSWITCH wired together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it all thats required to power up the MCU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not connected the 1P8OUT back to the VDD0 and VDD1 pins. Is there any issues with not doing that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are the implications if VDD0 and 1 are in the NC state?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have connected VDDA, VREFH to 1P8OUT. Will that suffice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kiran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Jan 2020 07:43:15 GMT</pubDate>
    <dc:creator>kiransajeev</dc:creator>
    <dc:date>2020-01-11T07:43:15Z</dc:date>
    <item>
      <title>KW36A BUCK AUTOSTART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW36A-BUCK-AUTOSTART/m-p/996733#M55818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use KW36A chip in buck auto start mode. I have the VDCDCIN and DCDC-CFG and PSWITCH wired together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it all thats required to power up the MCU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not connected the 1P8OUT back to the VDD0 and VDD1 pins. Is there any issues with not doing that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are the implications if VDD0 and 1 are in the NC state?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have connected VDDA, VREFH to 1P8OUT. Will that suffice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kiran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2020 07:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW36A-BUCK-AUTOSTART/m-p/996733#M55818</guid>
      <dc:creator>kiransajeev</dc:creator>
      <dc:date>2020-01-11T07:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: KW36A BUCK AUTOSTART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW36A-BUCK-AUTOSTART/m-p/996734#M55819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you need the VDD_0 and the VDD_1 connection. For further details, you can seen in our &lt;A href="https://www.nxp.com/docs/en/user-guide/MiniBoMKW36UG.pdf" title="https://www.nxp.com/docs/en/user-guide/MiniBoMKW36UG.pdf"&gt;FRDM-KW36 Minimum BoM Development BoardUser’s Guide&lt;/A&gt; , in chapter 3 the connections needed for the requested configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95995iB13F822BC130AA57/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 16:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW36A-BUCK-AUTOSTART/m-p/996734#M55819</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-01-16T16:52:34Z</dc:date>
    </item>
  </channel>
</rss>