<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does MKE18F512VLH16 Support P Flash Firmware Swapping? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-MKE18F512VLH16-Support-P-Flash-Firmware-Swapping/m-p/995297#M55770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you mention, this application note shouldn't be there. For example, if you check the reference manual from the K24 this has&amp;nbsp;a Swap Control command that it's mention in this application note.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will report this to the applications team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jan 2020 21:34:04 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-01-13T21:34:04Z</dc:date>
    <item>
      <title>Does MKE18F512VLH16 Support P Flash Firmware Swapping?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-MKE18F512VLH16-Support-P-Flash-Firmware-Swapping/m-p/995296#M55769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to take advantage of the P Flash swapping mechanism that is mentioned in AN4533&lt;SPAN&gt;(Robust Over-the-Air Firmware Updates Using Program FlashMemory Swap on Kinetis Microcontrollers).&amp;nbsp; I found this App Note from section 17.7 of the KE1xF manual, which leads me to believe that the MKE18F512VLH16 supports this.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Reading through the app note, it says that a device needs to have at least two P Flash blocks, and swapping capabilities.&amp;nbsp; The KE1xF manual mentions that the device has 2 256KB blocks in section 13.2.2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However looking at the PFLSH field in the FTFE_FCNFG register, it says that the only FTFE configuration that you can have is to support one program flash block and one FlexNVM block.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104800i496B5E6E17E424D5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am very confused as to why the manual would reference this app note if I did not even have the ability to do this in the first place.&amp;nbsp; I also do not see the FTFE FCCOB0 command for swapping (0x46) in the KE1xF manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am just looking for some clarification on whether the MKE18F512VLH16 supports P Flash swapping.&amp;nbsp; I have two P Flash blocks, and the reference manual refers to this app note.&amp;nbsp; However, I can only support one P Flash block, and have no reference to the command in the manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2020 00:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-MKE18F512VLH16-Support-P-Flash-Firmware-Swapping/m-p/995296#M55769</guid>
      <dc:creator>sean_dvorscak</dc:creator>
      <dc:date>2020-01-11T00:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: Does MKE18F512VLH16 Support P Flash Firmware Swapping?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-MKE18F512VLH16-Support-P-Flash-Firmware-Swapping/m-p/995297#M55770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you mention, this application note shouldn't be there. For example, if you check the reference manual from the K24 this has&amp;nbsp;a Swap Control command that it's mention in this application note.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will report this to the applications team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 21:34:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-MKE18F512VLH16-Support-P-Flash-Firmware-Swapping/m-p/995297#M55770</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-01-13T21:34:04Z</dc:date>
    </item>
  </channel>
</rss>