<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K22-120: Can VDD=1.8V if using USB interface? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-Can-VDD-1-8V-if-using-USB-interface/m-p/991609#M55707</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a K22-120 design.&amp;nbsp; I need the USB (device only) interface but also have a bunch of GPIO that needs to be 1.8V.&amp;nbsp; Can I power the USB via the VREGIN with 5V, but connect the VDD pins to a 1.8V power supply such that all of my GPIO (I2C, SPI, etc..) will be 1.8V.&amp;nbsp; I am trying to avoid level translators on my gpio for space reasons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2019 16:57:37 GMT</pubDate>
    <dc:creator>matthew_pattiso</dc:creator>
    <dc:date>2019-10-31T16:57:37Z</dc:date>
    <item>
      <title>K22-120: Can VDD=1.8V if using USB interface?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-Can-VDD-1-8V-if-using-USB-interface/m-p/991609#M55707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a K22-120 design.&amp;nbsp; I need the USB (device only) interface but also have a bunch of GPIO that needs to be 1.8V.&amp;nbsp; Can I power the USB via the VREGIN with 5V, but connect the VDD pins to a 1.8V power supply such that all of my GPIO (I2C, SPI, etc..) will be 1.8V.&amp;nbsp; I am trying to avoid level translators on my gpio for space reasons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 16:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-Can-VDD-1-8V-if-using-USB-interface/m-p/991609#M55707</guid>
      <dc:creator>matthew_pattiso</dc:creator>
      <dc:date>2019-10-31T16:57:37Z</dc:date>
    </item>
    <item>
      <title>Re: K22-120: Can VDD=1.8V if using USB interface?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-Can-VDD-1-8V-if-using-USB-interface/m-p/991610#M55708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;yes, it can. VREGIN should connect to USB VBUS, but VOUT33 connect to ground with a capacitor. Then you can connect VDD to 1.8v.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 08:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-Can-VDD-1-8V-if-using-USB-interface/m-p/991610#M55708</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-11-01T08:27:57Z</dc:date>
    </item>
  </channel>
</rss>