<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Build SDA Image in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991602#M55705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you downloading ZIP folder? Please check the following note in the guide you are following.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The code is found in the&amp;nbsp;MBED git repository, so it can be downloaded using a git clone command:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;“git clone&amp;nbsp;&lt;A href="https://github.com/mbedmicro/CMSIS-DAP.git"&gt;https://github.com/mbedmicro/CMSIS-DAP.git&lt;/A&gt;”&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note that there is a Download Zip option, but you will run into a issue when trying to compile that version, so you must download it via git instead.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Maybe that is the issue you are facing on your side. If not, please provide detailed description of the steps you are following.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2020 16:04:45 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2020-02-25T16:04:45Z</dc:date>
    <item>
      <title>Build SDA Image</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991601#M55704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to build the binary image for SDAV2 following the link&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded the Python v2.7 and the uVision V5.29&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also from github the&amp;nbsp;CMSIS-DAP-master&lt;/P&gt;&lt;P&gt;I follow the suggestion of installing the legacy pack, since I get the documented errors.&lt;/P&gt;&lt;P&gt;The python is on the path.&lt;/P&gt;&lt;P&gt;I get the following&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Build started: Project: k20dx128_bootloader&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Build target 'k20dx128_bootloader'&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Before Build - User command #1: python ..\..\..\tools\pre_build_script.py&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;'git' is not recognized as an internal or external command,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;operable program or batch file.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;#&amp;gt; Pre-build script start&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;#&amp;gt; No git version file to remove&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;#&amp;gt; Getting git SHA&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;#&amp;gt; ERROR: Failed to get git SHA, do you have git.exe in your PATH environment variable?&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;compiling version.c...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;..\..\Common\inc\mbed_htm.h(19): error: #5: cannot open source input file "version_git.h": No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; #include "version_git.h"&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;..\..\Common\src\version.c: 0 warnings, 1 error&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;".\Obj\k20dx128_bootloader.axf" - 1 Error(s), 0 Warning(s).&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Target not created.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Build Time Elapsed: 00:00:01&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A help is welcome&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 12:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991601#M55704</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2020-02-20T12:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: Build SDA Image</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991602#M55705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you downloading ZIP folder? Please check the following note in the guide you are following.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The code is found in the&amp;nbsp;MBED git repository, so it can be downloaded using a git clone command:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;“git clone&amp;nbsp;&lt;A href="https://github.com/mbedmicro/CMSIS-DAP.git"&gt;https://github.com/mbedmicro/CMSIS-DAP.git&lt;/A&gt;”&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note that there is a Download Zip option, but you will run into a issue when trying to compile that version, so you must download it via git instead.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Maybe that is the issue you are facing on your side. If not, please provide detailed description of the steps you are following.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2020 16:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991602#M55705</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-02-25T16:04:45Z</dc:date>
    </item>
    <item>
      <title>Re: Build SDA Image</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991603#M55706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You..&lt;/P&gt;&lt;P&gt;I am trying to proceed...&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 10:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Build-SDA-Image/m-p/991603#M55706</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2020-03-26T10:44:43Z</dc:date>
    </item>
  </channel>
</rss>