<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックNew KL03z is in secure mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-KL03z-is-in-secure-mode/m-p/990056#M55659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just got a new custom board with a KL03z chip. Unfortunately I am not able to flash it, because it is SECURE. I connected the chip via UART tried "flash-erase-all" with blhost and the Kinetis Flash Tool, which fails due to the secure state. "flash-erase-all-unsecure" is an unknown command. Is there anything I can do to unsecure the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bonus question: what could have happened to the chip? The assembler of the PCB should not have connected the chip to anything, as there weren't even wires connected. The chip should have come directly from production and not pre-flashed. Is it possible, that some electromagnetic discharge or something of the like accidently secured my chip? Keep in mind that a connection with the Kinetis Flash Tool is possible, and error codes are transmitted, so not all of the communication is broken.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Dec 2019 10:09:01 GMT</pubDate>
    <dc:creator>annika_huebner</dc:creator>
    <dc:date>2019-12-17T10:09:01Z</dc:date>
    <item>
      <title>New KL03z is in secure mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-KL03z-is-in-secure-mode/m-p/990056#M55659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just got a new custom board with a KL03z chip. Unfortunately I am not able to flash it, because it is SECURE. I connected the chip via UART tried "flash-erase-all" with blhost and the Kinetis Flash Tool, which fails due to the secure state. "flash-erase-all-unsecure" is an unknown command. Is there anything I can do to unsecure the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bonus question: what could have happened to the chip? The assembler of the PCB should not have connected the chip to anything, as there weren't even wires connected. The chip should have come directly from production and not pre-flashed. Is it possible, that some electromagnetic discharge or something of the like accidently secured my chip? Keep in mind that a connection with the Kinetis Flash Tool is possible, and error codes are transmitted, so not all of the communication is broken.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 10:09:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-KL03z-is-in-secure-mode/m-p/990056#M55659</guid>
      <dc:creator>annika_huebner</dc:creator>
      <dc:date>2019-12-17T10:09:01Z</dc:date>
    </item>
    <item>
      <title>Re: New KL03z is in secure mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-KL03z-is-in-secure-mode/m-p/990057#M55660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Here are some action could cause lock.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;1.The power is unstable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;2.Have not power down the chip when&amp;nbsp; plug the debuger&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;3.etc.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;You can use a j-link-command "unlock kinetis " to unlock the chip. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Jianyu:&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 2.0pt 0cm 2.0pt 0cm;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Have a great day,&lt;BR /&gt; TIC&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 2.0pt 0cm 2.0pt 0cm;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 2.0pt 0cm 2.0pt 0cm;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt; Note:&lt;BR /&gt; - If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 2.0pt 0cm 2.0pt 0cm;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 2.0pt 0cm 2.0pt 0cm;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;BR /&gt; -------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 03:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-KL03z-is-in-secure-mode/m-p/990057#M55660</guid>
      <dc:creator>nxf58904</dc:creator>
      <dc:date>2019-12-18T03:46:46Z</dc:date>
    </item>
  </channel>
</rss>