<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can NOT write in UART0 data register D in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985118#M55530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While trying to send data byte through UART0, an by writing this data byte to D register, the content of data register D doesn't change and always has a zero value 0x00. What is the problem here? There are a snapshots show that. Also TC and TDRE always set to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pp3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101810i18CA505A1AE85EC7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pp3.PNG" alt="pp3.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pp3.1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101820iF86B23370105183C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pp3.1.PNG" alt="pp3.1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jan 2020 10:54:42 GMT</pubDate>
    <dc:creator>muhammedhafez98</dc:creator>
    <dc:date>2020-01-08T10:54:42Z</dc:date>
    <item>
      <title>Can NOT write in UART0 data register D</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985118#M55530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While trying to send data byte through UART0, an by writing this data byte to D register, the content of data register D doesn't change and always has a zero value 0x00. What is the problem here? There are a snapshots show that. Also TC and TDRE always set to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pp3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101810i18CA505A1AE85EC7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pp3.PNG" alt="pp3.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pp3.1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101820iF86B23370105183C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pp3.1.PNG" alt="pp3.1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 10:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985118#M55530</guid>
      <dc:creator>muhammedhafez98</dc:creator>
      <dc:date>2020-01-08T10:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can NOT write in UART0 data register D</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985119#M55531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The data register is used to write data to that is to be sent and read data that is received. That is, unless you have a loop-back where the data your send is received, you won't see the value that was written (you will see the last data that was received).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should however see the written data being sent out on the Tx pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;(uTasker project developer for Kinetis and i.MX RT)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2020 00:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985119#M55531</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-01-09T00:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: Can NOT write in UART0 data register D</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985120#M55532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition, if you'd like to be able to better manage those values. You can create a buffer, that stores the values being read from this register.&lt;/P&gt;&lt;P&gt;Then compare your buffers to confirm if the data is being written correctly.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 18:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-NOT-write-in-UART0-data-register-D/m-p/985120#M55532</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-01-13T18:22:24Z</dc:date>
    </item>
  </channel>
</rss>