<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MK60DN512VLL10R MCU USB power pins in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983853#M55520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;If you don't&amp;nbsp; use USB, both VOUT33 and VREGIN should tie to output and ground through 10k resistor. If you still need USB but not use VOUT33, you can refer to &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/965047?commentID=965047#comment-965047" title="https://community.nxp.com/message/965047?commentID=965047#comment-965047"&gt;https://community.nxp.com/message/965047?commentID=965047#comment-965047&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't use USB, VOUT33 connect with a 10uF cap will not cause any problem.&lt;/P&gt;&lt;P&gt;But if you still use USB, the above link will give you some answer too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jan 2020 03:20:04 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2020-01-22T03:20:04Z</dc:date>
    <item>
      <title>MK60DN512VLL10R MCU USB power pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983852#M55519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We intend to use NXP’s MK60DN512VLL10R MCU in a new product. Can we leave pins 12 (VOUT33) &amp;amp; 13 (VREGIN) disconnected(floating). We do &lt;EM style="text-decoration: underline; "&gt;not&lt;/EM&gt; intend to use USB power. Also, the datasheet states that pin 12 should/must have a capacitor attached. But, it can’t be more than 8.16uF. We are shipping product with 10uF on this pin. What kind of problems could this cause?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 16:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983852#M55519</guid>
      <dc:creator>markheiberger</dc:creator>
      <dc:date>2020-01-21T16:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512VLL10R MCU USB power pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983853#M55520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;If you don't&amp;nbsp; use USB, both VOUT33 and VREGIN should tie to output and ground through 10k resistor. If you still need USB but not use VOUT33, you can refer to &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/965047?commentID=965047#comment-965047" title="https://community.nxp.com/message/965047?commentID=965047#comment-965047"&gt;https://community.nxp.com/message/965047?commentID=965047#comment-965047&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't use USB, VOUT33 connect with a 10uF cap will not cause any problem.&lt;/P&gt;&lt;P&gt;But if you still use USB, the above link will give you some answer too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 03:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983853#M55520</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-01-22T03:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512VLL10R MCU USB power pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983854#M55521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this note from the product literature is no longer correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 18:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983854#M55521</guid>
      <dc:creator>markheiberger</dc:creator>
      <dc:date>2020-01-22T18:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: MK60DN512VLL10R MCU USB power pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983855#M55522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, this is noted on the reference manual. Then floating those pins please. May other kinetis device datasheet says tie to ground via 10k resistor, like k22 and k64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jan 2020 07:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK60DN512VLL10R-MCU-USB-power-pins/m-p/983855#M55522</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-01-25T07:36:25Z</dc:date>
    </item>
  </channel>
</rss>