<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Baremetal SDK for K64</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Baremetal-SDK-for-K64/m-p/980802#M55484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't activate FreeRTOS the Kinetis SDK is "bare-metal" since it just runs in a forever loop.&lt;BR /&gt;There are also IAR project I believe in the examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See also the uTasker project for an alternative SDK with complete IAR K64 project (rather than various example) and Kinetis chip simulation in Visual Studio. It has a cooperative scheduler, FreeRTOS and bare-metal options (last only recommended for simple projects though and not for TCP/IP, USB stack etc.).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Feb 2020 16:52:40 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-02-04T16:52:40Z</dc:date>
    <item>
      <title>Baremetal SDK for K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Baremetal-SDK-for-K64/m-p/980801#M55483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Just wondering whether it is possible to get a baremetal SDK for K64 custom board(IAR IDE). Only because I am not used to this OS running on controllers. I had gone through the SDK and MCUXpresso config method. All looks interesting. But since I could not find any article with baremetal SDK for IAR this post is being put up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 13:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Baremetal-SDK-for-K64/m-p/980801#M55483</guid>
      <dc:creator>sionp</dc:creator>
      <dc:date>2020-02-04T13:15:56Z</dc:date>
    </item>
    <item>
      <title>Re: Baremetal SDK for K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Baremetal-SDK-for-K64/m-p/980802#M55484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't activate FreeRTOS the Kinetis SDK is "bare-metal" since it just runs in a forever loop.&lt;BR /&gt;There are also IAR project I believe in the examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See also the uTasker project for an alternative SDK with complete IAR K64 project (rather than various example) and Kinetis chip simulation in Visual Studio. It has a cooperative scheduler, FreeRTOS and bare-metal options (last only recommended for simple projects though and not for TCP/IP, USB stack etc.).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 16:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Baremetal-SDK-for-K64/m-p/980802#M55484</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-02-04T16:52:40Z</dc:date>
    </item>
  </channel>
</rss>