<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: What is the double week mechanism?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975469#M55314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95177i237BAA8DF00C2E04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Nov 2019 02:32:51 GMT</pubDate>
    <dc:creator>nxf56274</dc:creator>
    <dc:date>2019-11-12T02:32:51Z</dc:date>
    <item>
      <title>What is the double week mechanism?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975468#M55313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using SDK_2.6.0_MKE04Z128xxx4.&lt;/P&gt;&lt;P&gt;Among them, there is a title on I2C-related driver sources.&lt;/P&gt;&lt;P&gt;What kind of mechanism do you point to specifically?&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;The place marked with (&amp;lt;--- ???).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*!&lt;BR /&gt; * brief Initializes the I2C handle which is used in transactional functions.&lt;BR /&gt; *&lt;BR /&gt; * param base I2C base pointer.&lt;BR /&gt; * param handle pointer to i2c_master_handle_t structure to store the transfer state.&lt;BR /&gt; * param callback pointer to user callback function.&lt;BR /&gt; * param userData user parameter passed to the callback function.&lt;BR /&gt; */&lt;BR /&gt;void I2C_MasterTransferCreateHandle(I2C_Type *base,&lt;BR /&gt; i2c_master_handle_t *handle,&lt;BR /&gt; i2c_master_transfer_callback_t callback,&lt;BR /&gt; void *userData)&lt;BR /&gt;{&lt;BR /&gt; assert(NULL != handle);&lt;/P&gt;&lt;P&gt;uint32_t instance = I2C_GetInstance(base);&lt;/P&gt;&lt;P&gt;/* Zero handle. */&lt;BR /&gt; (void)memset(handle, 0, sizeof(*handle));&lt;/P&gt;&lt;P&gt;/* Set callback and userData. */&lt;BR /&gt; handle-&amp;gt;completionCallback = callback;&lt;BR /&gt; handle-&amp;gt;userData = userData;&lt;/P&gt;&lt;P&gt;/* Save the context in global variables to support the double weak mechanism. */　&amp;lt;--- ???&lt;BR /&gt; s_i2cHandle[instance] = handle;&lt;/P&gt;&lt;P&gt;/* Save master interrupt handler. */&lt;BR /&gt; s_i2cMasterIsr = I2C_MasterTransferHandleIRQ;&lt;/P&gt;&lt;P&gt;/* Enable NVIC interrupt. */&lt;BR /&gt; (void)EnableIRQ(s_i2cIrqs[instance]);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am always grateful for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 01:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975468#M55313</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-11-12T01:28:47Z</dc:date>
    </item>
    <item>
      <title>Re: What is the double week mechanism?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975469#M55314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95177i237BAA8DF00C2E04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 02:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975469#M55314</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2019-11-12T02:32:51Z</dc:date>
    </item>
    <item>
      <title>Re: What is the double week mechanism?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975470#M55315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;BR /&gt;The two layers are talking about interrupt flow.&lt;BR /&gt;I fully understood.&lt;BR /&gt;Have a nice day&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 03:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-double-week-mechanism/m-p/975470#M55315</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-11-12T03:28:56Z</dc:date>
    </item>
  </channel>
</rss>