<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMKW41Z - Debugger disconnects when VDD1P8 is increased</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974826#M55302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running a custom board with MKW41Z on it, powered from 3V3. In my hardware initialization routine (inspired from the FRDM-MKW41 examples), I'm increasing the output voltage of the built-in DC regulator from 1.8V to 2.6V. When that change takes effect, the board continues to run as expected, but the debugger (an LPCXpresso LPCLink 2) disconnects and the IDE (MCUXpresso 10.2.1)&amp;nbsp; throws an error and the debug session stops. The board continues to function as expected. Then I have to reset the board a couple of times until I'm able to erase the flash and reconnect with the debugger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jan 2020 18:43:35 GMT</pubDate>
    <dc:creator>alexx_88</dc:creator>
    <dc:date>2020-01-17T18:43:35Z</dc:date>
    <item>
      <title>MKW41Z - Debugger disconnects when VDD1P8 is increased</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974826#M55302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running a custom board with MKW41Z on it, powered from 3V3. In my hardware initialization routine (inspired from the FRDM-MKW41 examples), I'm increasing the output voltage of the built-in DC regulator from 1.8V to 2.6V. When that change takes effect, the board continues to run as expected, but the debugger (an LPCXpresso LPCLink 2) disconnects and the IDE (MCUXpresso 10.2.1)&amp;nbsp; throws an error and the debug session stops. The board continues to function as expected. Then I have to reset the board a couple of times until I'm able to erase the flash and reconnect with the debugger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 18:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974826#M55302</guid>
      <dc:creator>alexx_88</dc:creator>
      <dc:date>2020-01-17T18:43:35Z</dc:date>
    </item>
    <item>
      <title>Re: MKW41Z - Debugger disconnects when VDD1P8 is increased</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974827#M55303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandru, I hope you're doing well!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please try attaching the debug probe after the voltage change is performed to see if it can connect and continue the debug session?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can be done while the probe is connected to your board, by choosing this option in MCUXpresso:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97382i83F35F35B75F53DF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you still have issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 16:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974827#M55303</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-01-21T16:29:21Z</dc:date>
    </item>
    <item>
      <title>Re: MKW41Z - Debugger disconnects when VDD1P8 is increased</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974828#M55304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, will try this and let you know :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2020 22:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW41Z-Debugger-disconnects-when-VDD1P8-is-increased/m-p/974828#M55304</guid>
      <dc:creator>alexx_88</dc:creator>
      <dc:date>2020-02-28T22:36:44Z</dc:date>
    </item>
  </channel>
</rss>