<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KV46F256 flash write acces pb when interrupt activated in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46F256-flash-write-acces-pb-when-interrupt-activated/m-p/972156#M55266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Step through the interrupt(s) that are executed during flashing operations to ensure that no flash access is being performed by them.&lt;/P&gt;&lt;P&gt;- Beware that if they access consts these probably are in Flash and so need to be declared as initialsed variables instead&lt;BR /&gt;- You may find that the code calls library routines (eg. for arithmetic operations or even for memory initialisation in subroutines) and these will also need to be located to SRAM or the code modified in order to avoid the use of such calls (eg. GCC sometimes calls memset() to initialise a buffer declared as &lt;SPAN style="font-family: courier new, courier, monospace;"&gt;unsigned char ucBuffer[10] = {0};&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;&lt;EM&gt;Complete Kinetis solutions for professional needs, training and support:http://www.utasker.com/kinetis.html&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000080;"&gt;&lt;EM&gt;uTasker: supporting &amp;gt;1'000 registered Kinetis users get products faster and cheaper to market&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000000;"&gt;&lt;EM&gt;Request Free emergency remote desk-top consulting at &lt;A href="http://www.utasker.com/services.html" target="test_blank"&gt;http://www.utasker.com/services.html&lt;/A&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2019 11:15:43 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2019-06-11T11:15:43Z</dc:date>
    <item>
      <title>KV46F256 flash write acces pb when interrupt activated</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46F256-flash-write-acces-pb-when-interrupt-activated/m-p/972155#M55265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone&lt;/P&gt;&lt;P&gt;I've a problem: I am using KV46F256VLL16&amp;nbsp;on MCUXPRESSO environment&lt;/P&gt;&lt;P&gt;I have to store periodically some parameters in&amp;nbsp;Flash memory.&lt;/P&gt;&lt;P&gt;In a first step, when I disable the interrupt the writing in flash goes well (Erase / VerifyErase / Program / VerifyProgram sequence)&lt;/P&gt;&lt;P&gt;I would like to keep my interrupt activated during the writing.&lt;/P&gt;&lt;P&gt;I build a RAM_vector section as described in the forum&lt;/P&gt;&lt;P&gt;where I already&amp;nbsp;moved interrupt section from&amp;nbsp;FLASH to RAM first =&amp;gt; (I always need to inactivate interrupt to make it working well - interrupt running well in RAM )&lt;/P&gt;&lt;P&gt;Secondly,&amp;nbsp;I moved the code of interrupt from&amp;nbsp;FLASH to RAM also =&amp;gt; (same result - code running well in RAM&amp;nbsp;but access to flash write not possible with interrupt&amp;nbsp;activated)&lt;/P&gt;&lt;P&gt;(I use&amp;nbsp;read carefully&amp;nbsp;the AN4695 / AN4507)&lt;/P&gt;&lt;P&gt;I still get a boot when I try to pass a flash write command when interrupt are activated - any idea ?&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 10:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46F256-flash-write-acces-pb-when-interrupt-activated/m-p/972155#M55265</guid>
      <dc:creator>merigotbertrand</dc:creator>
      <dc:date>2019-06-11T10:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: KV46F256 flash write acces pb when interrupt activated</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46F256-flash-write-acces-pb-when-interrupt-activated/m-p/972156#M55266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Step through the interrupt(s) that are executed during flashing operations to ensure that no flash access is being performed by them.&lt;/P&gt;&lt;P&gt;- Beware that if they access consts these probably are in Flash and so need to be declared as initialsed variables instead&lt;BR /&gt;- You may find that the code calls library routines (eg. for arithmetic operations or even for memory initialisation in subroutines) and these will also need to be located to SRAM or the code modified in order to avoid the use of such calls (eg. GCC sometimes calls memset() to initialise a buffer declared as &lt;SPAN style="font-family: courier new, courier, monospace;"&gt;unsigned char ucBuffer[10] = {0};&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;&lt;EM&gt;Complete Kinetis solutions for professional needs, training and support:http://www.utasker.com/kinetis.html&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000080;"&gt;&lt;EM&gt;uTasker: supporting &amp;gt;1'000 registered Kinetis users get products faster and cheaper to market&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000000;"&gt;&lt;EM&gt;Request Free emergency remote desk-top consulting at &lt;A href="http://www.utasker.com/services.html" target="test_blank"&gt;http://www.utasker.com/services.html&lt;/A&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 11:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46F256-flash-write-acces-pb-when-interrupt-activated/m-p/972156#M55266</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-06-11T11:15:43Z</dc:date>
    </item>
  </channel>
</rss>