<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How can I connect the DEVKIT-ZVL128 to Freemaster?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971070#M55225</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot, it works with the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;STRONG&gt;P&amp;amp;E HCS12Z&lt;/STRONG&gt;&amp;nbsp;configuration but i seem to run into another problem, because I'm using the &lt;STRONG&gt;devkit-zvl128&lt;/STRONG&gt;&amp;nbsp;connected to a &lt;STRONG&gt;TouchPAD&amp;nbsp;&lt;/STRONG&gt;i want to measure the touch with freemaster, the problem is that freemaster can't detect the touch even tought the program I'm using turns on a LED when i touch one of the electrodes of the PAD and the freemaster program has the electrodes variables so the measure should appear but&amp;nbsp; it doesn't.&amp;nbsp;What can i do.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jul 2019 20:14:55 GMT</pubDate>
    <dc:creator>efrain_castro</dc:creator>
    <dc:date>2019-07-29T20:14:55Z</dc:date>
    <item>
      <title>How can I connect the DEVKIT-ZVL128 to Freemaster?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971068#M55223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When i open the &lt;STRONG&gt;.pmp&lt;/STRONG&gt; program that opens Freemaster and then i press the &lt;STRONG&gt;GO!&lt;/STRONG&gt; icon a window appears telling me that the DEVKIT-ZVL128 is not connected then i press the &lt;STRONG&gt;Use Wizard&lt;/STRONG&gt; so i can configure the connection, i&amp;nbsp;choose the&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Use direct connection to on-board USB port&lt;/STRONG&gt; then when choosing baud rate i&amp;nbsp;choose 9600 and 115200 so it can connect but another windows appears saying &lt;STRONG&gt;No board detected on any specified UART communication ports&lt;/STRONG&gt; even though&amp;nbsp;i have the board connected and it appears on the Probing UART Ports.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84496i7907297FC4A437DB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.jpg" alt="pastedImage_7.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 18:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971068#M55223</guid>
      <dc:creator>efrain_castro</dc:creator>
      <dc:date>2019-07-25T18:11:16Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect the DEVKIT-ZVL128 to Freemaster?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971069#M55224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume that your board is connected through the OSBDM or BDM interface.&lt;/P&gt;&lt;P&gt;Please follow the steps below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Go to menu Tools -&amp;gt; Connection Wizard -&amp;gt; Next&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Choose the "Connect through a debugger probe or on-board debugger interface" -&amp;gt; Next -&amp;gt; Next&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86212i1C34B2CFE065F227/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. Click on the Plug-in Configuration&lt;/P&gt;&lt;P&gt;4. Select " P&amp;amp;E OSBDM" or "P&amp;amp;E HCS12Z" (it depends which interface you use), after that you can Test Connection -&amp;gt; Ok -&amp;gt; Ok -&amp;gt; Finish&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that, it should be connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jul 2019 08:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971069#M55224</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-07-29T08:33:36Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect the DEVKIT-ZVL128 to Freemaster?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971070#M55225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot, it works with the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;STRONG&gt;P&amp;amp;E HCS12Z&lt;/STRONG&gt;&amp;nbsp;configuration but i seem to run into another problem, because I'm using the &lt;STRONG&gt;devkit-zvl128&lt;/STRONG&gt;&amp;nbsp;connected to a &lt;STRONG&gt;TouchPAD&amp;nbsp;&lt;/STRONG&gt;i want to measure the touch with freemaster, the problem is that freemaster can't detect the touch even tought the program I'm using turns on a LED when i touch one of the electrodes of the PAD and the freemaster program has the electrodes variables so the measure should appear but&amp;nbsp; it doesn't.&amp;nbsp;What can i do.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jul 2019 20:14:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971070#M55225</guid>
      <dc:creator>efrain_castro</dc:creator>
      <dc:date>2019-07-29T20:14:55Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect the DEVKIT-ZVL128 to Freemaster?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971071#M55226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Forget it i used a P&amp;amp;E micro multilink universal for&amp;nbsp; the measure thanks you because the configuration is the same.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 16:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-can-I-connect-the-DEVKIT-ZVL128-to-Freemaster/m-p/971071#M55226</guid>
      <dc:creator>efrain_castro</dc:creator>
      <dc:date>2019-07-31T16:15:02Z</dc:date>
    </item>
  </channel>
</rss>