<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: problem starting to use frdm-kl05z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236991#M5516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you open CodeWarrior10.5 , the workspace you should select is like this:E:\Program Files\KL05-SC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Dec 2013 02:25:04 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2013-12-02T02:25:04Z</dc:date>
    <item>
      <title>problem starting to use frdm-kl05z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236990#M5515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;follow the sample code guide for codewarrior to load the LED_Blink project, first import the workspace as&lt;STRONG&gt; &lt;SPAN style="color: #ff0000;"&gt;..\ klxx‐sc‐baremetal\build\cw\LED_Blink&lt;/SPAN&gt;&lt;/STRONG&gt;, then import the project by setting the root directory also as&amp;nbsp; &lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;..\ klxx‐sc‐baremetal\build\cw\LED_Blink&lt;/STRONG&gt;&lt;/SPAN&gt; according to the guid, however when push the finish button error occurs, saying that&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;Invalid project description.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;&amp;nbsp; D:\Project\Freescale\Software\KL05-SC\klxx-sc-baremetal\build\cw\LED_Blink overlaps the workspace location: D:\Project\Freescale\Software\KL05-SC\klxx-sc-baremetal\build\cw\LED_Blink&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using codewarrior 10.5, anyone knows what the problem is?&lt;/P&gt;&lt;P&gt;otherwise the guide says that a script to help clone project settings is available, but i can only find them in the iar and keil directory, there isn't a &lt;SPAN style="color: #ff0000;"&gt;make_new_cw_project.exe file &lt;/SPAN&gt;in the cw directory as described.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Nov 2013 04:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236990#M5515</guid>
      <dc:creator>northgod</dc:creator>
      <dc:date>2013-11-30T04:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: problem starting to use frdm-kl05z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236991#M5516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you open CodeWarrior10.5 , the workspace you should select is like this:E:\Program Files\KL05-SC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 02:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236991#M5516</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2013-12-02T02:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: problem starting to use frdm-kl05z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236992#M5517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response. However I could not find the file&lt;/P&gt;&lt;P&gt;make_new_cw_project.exe mentioned in the readme.txt in sample code&lt;/P&gt;&lt;P&gt;directory. Can I use the make_new_project.exe under IAR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2013/12/2 Robin_Shen &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE level="1"&gt;&lt;P&gt;       &amp;lt;https://community.freescale.com/&amp;gt;  problem starting to use frdm-kl05z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Robin_Shen&amp;lt;https://community.freescale.com/people/Robin_Shen?et=watches.email.thread&amp;gt;in *&lt;/P&gt;&lt;P&gt;Kinetis Microcontrollers* - View the full discussion&amp;lt;https://community.freescale.com/message/366052?et=watches.email.thread#366052&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 04:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236992#M5517</guid>
      <dc:creator>northgod</dc:creator>
      <dc:date>2013-12-02T04:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: Re: problem starting to use frdm-kl05z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236993#M5518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think you can use the make_new_project in IAR folder if you use CW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can have a try according to these steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Copy the whole project folder into workspace.&lt;BR /&gt;In Project folder, drag .project directly to CodeWarrior "CodeWarrior Projects" window.&lt;BR /&gt;Then, you will see the project was imported. Right click the project name and then "Clean" before building.&lt;BR /&gt;If the project works before, then, this imported project should be built with success.&lt;/P&gt;&lt;P&gt;If you want to rename the project, then, just right the project and click "Rename".&lt;BR /&gt;CodeWarrior will create a duplicated project for it and then give it the new name.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 08:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236993#M5518</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2013-12-02T08:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: problem starting to use frdm-kl05z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236994#M5519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why is this so difficult to create "demo" projects!?&amp;nbsp; It seems that freescale would take the time to create projects for each of the platforms IAR/CW etc if you are going to create code for them.&amp;nbsp; I have spend days trying to go through this process of re-creating a very simple and basic "demo" project is codewarrior. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code comes packaged in packaged and ready to install.&amp;nbsp; Why not make it so that we can actually build it in Codewarrior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just opened a thread on this very similar topic of how can I make the supplied code build in freescales tools.&amp;nbsp; Seems that this would not be too much to ask for.&amp;nbsp; Frustrated..... Very excited to learn the product though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321593"&gt;port example bare-metal source code to codewarrior project&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Mar 2014 22:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-starting-to-use-frdm-kl05z/m-p/236994#M5519</guid>
      <dc:creator>mbjvfx</dc:creator>
      <dc:date>2014-03-28T22:03:39Z</dc:date>
    </item>
  </channel>
</rss>