<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem in initialising DDR2 registers in freescale K70 twr in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-initialising-DDR2-registers-in-freescale-K70-twr/m-p/236823#M5506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;The query is as follows.&lt;/P&gt;&lt;P&gt;We are using K70 Twr and i need to test the DDR2 SDRAM memory connected to it. We are not using RTOS. The task is to test the DDR2 memory. I had used twr_ddr2_script_init() from the example project from the driver file sdram.c and it works in the example project and i am able to read and write to the memory.&lt;/P&gt;&lt;P&gt;Now when i try to read or write to the memory in our customized project ,we are not able to initialise the registers, it stops in CR_00 itself, also the junk value in the memory is overwritten with a value 0x23000042. Tried writing into write back (from 0x70000000) and write through(from 0x80000000) memory also. Please help with a solution.&lt;/P&gt;&lt;P&gt;I am attaching our project setting files and also the main which we are using to check our functionalities. It is a draft copy. Please help us with this.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337407"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337407"&gt;freescale.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Nov 2013 04:10:24 GMT</pubDate>
    <dc:creator>shanthipk</dc:creator>
    <dc:date>2013-11-30T04:10:24Z</dc:date>
    <item>
      <title>Problem in initialising DDR2 registers in freescale K70 twr</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-initialising-DDR2-registers-in-freescale-K70-twr/m-p/236823#M5506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;The query is as follows.&lt;/P&gt;&lt;P&gt;We are using K70 Twr and i need to test the DDR2 SDRAM memory connected to it. We are not using RTOS. The task is to test the DDR2 memory. I had used twr_ddr2_script_init() from the example project from the driver file sdram.c and it works in the example project and i am able to read and write to the memory.&lt;/P&gt;&lt;P&gt;Now when i try to read or write to the memory in our customized project ,we are not able to initialise the registers, it stops in CR_00 itself, also the junk value in the memory is overwritten with a value 0x23000042. Tried writing into write back (from 0x70000000) and write through(from 0x80000000) memory also. Please help with a solution.&lt;/P&gt;&lt;P&gt;I am attaching our project setting files and also the main which we are using to check our functionalities. It is a draft copy. Please help us with this.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337407"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337407"&gt;freescale.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Nov 2013 04:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-initialising-DDR2-registers-in-freescale-K70-twr/m-p/236823#M5506</guid>
      <dc:creator>shanthipk</dc:creator>
      <dc:date>2013-11-30T04:10:24Z</dc:date>
    </item>
  </channel>
</rss>