<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Acquisition FLEXIO/SD card</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957246#M54935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lacouture,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to answer your questions the best I can:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Acquisition: Flexio,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1) &amp;nbsp;What is the expected maximum input external Clock supported by the FlexIO peripheral for K80 (sampling)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87113i94450CD4B68C4F5C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the reference manual mention that the maximum core clock&amp;nbsp;can be used to supply&amp;nbsp;the FlexIO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;2) &amp;nbsp;Is there any other NXP micro that can support higher input external Clock than K80?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Other MCU that has the same features is the K28/K27, but it has the same core frequency. Other MCU that has this features is the i.MX RT 1050/1060, mybe you could take a look at it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This peripheral is used to emulate other protocols like I2C, SPI or other protocols. I don't really understand the relation between this and the sampling in the ADC, are you going&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Record: SD card controller&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;3) According to the SD card information, a micro SDXC SanDisk Extreme 128 Go can write data until 90 Mo/s. What could be the maximum writing speed that I can expect by using FatFs or blocks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In the reference manual it mention the maximum data transfer is 200 Mbps for 4 lines, and 416 Mbps for 8 lines.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87579iCFC86FE0A068EAF0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;4) Which SD card would you recommend me to use for having the best writing performance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Unforunately, NXP doesn't have a list or recommended SD to work with its harware but if the operating range is between the mentioned&amp;nbsp; in the Table 56. SDHC full voltage range switching specifications it should be ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2019 20:47:45 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-09-09T20:47:45Z</dc:date>
    <item>
      <title>Acquisition FLEXIO/SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957245#M54934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a project of data acquisition. I must store data from ADC into a micro SD card. The data are from 1 bit to 4 bits (0/, sampled by a configured external clock from 16MHz to 32 MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found the micro Kinetis K80 that could be a solution thanks to the Flexio and the SD card controller. I have some questions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Acquisition: Flexio,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) &amp;nbsp;What is the expected maximum input external Clock supported by the FlexIO peripheral for K80 (sampling)?&lt;/P&gt;&lt;P&gt;2) &amp;nbsp;Is there any other NXP micro that can support higher input external Clock than K80?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Record: SD card controller&lt;/P&gt;&lt;P&gt;3) According to the SD card information, a micro SDXC SanDisk Extreme 128 Go can write data until 90 Mo/s. What could be the maximum writing speed that I can expect by using FatFs or blocks.&lt;/P&gt;&lt;P&gt;4) Which SD card would you recommend me to use for having the best writing performance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2019 13:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957245#M54934</guid>
      <dc:creator>lacouturepatric</dc:creator>
      <dc:date>2019-09-06T13:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: Acquisition FLEXIO/SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957246#M54935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lacouture,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to answer your questions the best I can:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Acquisition: Flexio,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1) &amp;nbsp;What is the expected maximum input external Clock supported by the FlexIO peripheral for K80 (sampling)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87113i94450CD4B68C4F5C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the reference manual mention that the maximum core clock&amp;nbsp;can be used to supply&amp;nbsp;the FlexIO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;2) &amp;nbsp;Is there any other NXP micro that can support higher input external Clock than K80?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Other MCU that has the same features is the K28/K27, but it has the same core frequency. Other MCU that has this features is the i.MX RT 1050/1060, mybe you could take a look at it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This peripheral is used to emulate other protocols like I2C, SPI or other protocols. I don't really understand the relation between this and the sampling in the ADC, are you going&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Record: SD card controller&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;3) According to the SD card information, a micro SDXC SanDisk Extreme 128 Go can write data until 90 Mo/s. What could be the maximum writing speed that I can expect by using FatFs or blocks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In the reference manual it mention the maximum data transfer is 200 Mbps for 4 lines, and 416 Mbps for 8 lines.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87579iCFC86FE0A068EAF0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;4) Which SD card would you recommend me to use for having the best writing performance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Unforunately, NXP doesn't have a list or recommended SD to work with its harware but if the operating range is between the mentioned&amp;nbsp; in the Table 56. SDHC full voltage range switching specifications it should be ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 20:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957246#M54935</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-09-09T20:47:45Z</dc:date>
    </item>
    <item>
      <title>Re: Acquisition FLEXIO/SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957247#M54936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Hello Alexis,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Thank you very much for your answer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Acquisition: Flexio,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;I succeed to sample data at 21 MHz. For the test, I used an FPGA and the TWR-K80F150M. The clock and data were generated by an FPGA. The TWR-K80F150M capture the data (shifter) and the clk was used as Trigger. The software that I used was FLEXIO Camera example with the EDMA. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Do you think that 21 MHz is the upper limit for Flexio K80? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;W&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;hat is the expected maximum input external Clock supported by the FlexIO peripheral for i.MX RT 1050/1060?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Record: SD card controller&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;I think the 200 Mbps for 4 lines&lt;/SPAN&gt; will not be&amp;nbsp;&lt;SPAN style="display: inline !important; float: none; background-color: transparent; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px; word-wrap: break-word;"&gt;enough &lt;/SPAN&gt; for my application.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Do you have an example of MMC card using 8 parallel data than can accept a data transfer&lt;/SPAN&gt; at 416 Mbps?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Can I used an SD card UHS 2 for having a data transfer at 416 Mbps. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt;"&gt;Patrice&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 09:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957247#M54936</guid>
      <dc:creator>lacouturepatric</dc:creator>
      <dc:date>2019-09-12T09:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: Acquisition FLEXIO/SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957248#M54937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lacouture,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check my answers below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Do you think that 21 MHz is the upper limit for Flexio K80?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For K80, the limit is 25MHz.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;What is the expected maximum input external Clock supported by the FlexIO peripheral for i.MX RT 1050/1060?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The operating clock is limited to 120MHz so it should expect a similar&amp;nbsp;sample data&amp;nbsp;rate than the K80.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Do you have an example of MMC card using 8 parallel data than can accept a data transfer&amp;nbsp;at 416 Mbps?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Since this is for MMC it will not be the same since the SD Card only have 4 parallel lines.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Can I used an SD card UHS 2 for having a data transfer at 416 Mbps?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I think you could use it but the frequency at which the module work would not be enough to reach that speed.&lt;/P&gt;&lt;P&gt;For this the i.MX RT would be possible to use it since it has a better module than the K80.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 17:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957248#M54937</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-09-13T17:37:22Z</dc:date>
    </item>
    <item>
      <title>Re: Acquisition FLEXIO/SD card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957249#M54938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, thank you very much for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrice Lacouture&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 14:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Acquisition-FLEXIO-SD-card/m-p/957249#M54938</guid>
      <dc:creator>lacouturepatric</dc:creator>
      <dc:date>2019-10-02T14:43:49Z</dc:date>
    </item>
  </channel>
</rss>