<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-KEXX Driver Library Package in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954867#M54861</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;Unlike other kinetis device, KE0x set pin function in group. Register bit SIM-&amp;gt;PINSEL0. SPI0PS select SPI0 pin group. In the example, it write 1 to this bit. So, SPI0_SCK, SPI0_MOSI, SPI0_MISO, and SPI0_PCS are mapped on PTE0, PTE1, PTE2, and PTE3.&lt;/P&gt;&lt;P&gt;This library hasn't any documents. It's really not good. I prefer FRDM-KE06 SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 10:33:31 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-07-23T10:33:31Z</dc:date>
    <item>
      <title>FRDM-KEXX Driver Library Package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954865#M54859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run an SPI sample "SPI_MasterInt_demo"　of the FRDM-KE06Z board.　&lt;BR /&gt;I think a demo to send and receive, but where is the jumper pin connection of send-&amp;gt; receive described?&lt;/P&gt;&lt;P&gt;I'm not looking at the source code, so it would be helpful if I could explain it.&lt;BR /&gt;Also, is there a document that explains the connection and operation when running other sample drivers with FRDM-KE06Z?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 06:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954865#M54859</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-07-23T06:19:33Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEXX Driver Library Package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954866#M54860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82363i817A9B0C577C778C/image-size/large?v=v2&amp;amp;px=999" title="FRDM-KEXX Driver Library.jpg" alt="FRDM-KEXX Driver Library.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 08:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954866#M54860</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-07-23T08:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEXX Driver Library Package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954867#M54861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;Unlike other kinetis device, KE0x set pin function in group. Register bit SIM-&amp;gt;PINSEL0. SPI0PS select SPI0 pin group. In the example, it write 1 to this bit. So, SPI0_SCK, SPI0_MOSI, SPI0_MISO, and SPI0_PCS are mapped on PTE0, PTE1, PTE2, and PTE3.&lt;/P&gt;&lt;P&gt;This library hasn't any documents. It's really not good. I prefer FRDM-KE06 SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 10:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954867#M54861</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-07-23T10:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEXX Driver Library Package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954868#M54862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am always grateful for your help.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;As shown in the example of FRDM-KE06 SDK SPI (SDK_2.6.0_MKE04Z128xxx4 \ boards \ frdmke06z \ driver_examples \ spi \ interrupt_b2b_transfer \ master \ iar),&lt;/P&gt;&lt;P&gt;I connected J4 connector pins 3 and 5 of the FRDM board, and it worked well .&lt;BR /&gt;The following was displayed on the console:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;　　Master start ...&lt;BR /&gt;　　success&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is easy to understand.&lt;BR /&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun 　(Natori City, Miyagi Prefecture, Japan)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 00:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954868#M54862</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-07-24T00:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEXX Driver Library Package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954869#M54863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for your trust and appreciation!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 02:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEXX-Driver-Library-Package/m-p/954869#M54863</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-07-24T02:33:35Z</dc:date>
    </item>
  </channel>
</rss>