<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM_KL25Z problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-problem/m-p/944521#M54522</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have started some demo applications from SDK for FRDM_KL25Z. when I run demo for UART I can not fire LED diodes, and when I started LED demo I can not start UART in that application. What should I do to get UART functionalities in LED application and vice versa?&lt;BR /&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 08:10:02 GMT</pubDate>
    <dc:creator>mato_cica1</dc:creator>
    <dc:date>2019-07-05T08:10:02Z</dc:date>
    <item>
      <title>FRDM_KL25Z problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-problem/m-p/944521#M54522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have started some demo applications from SDK for FRDM_KL25Z. when I run demo for UART I can not fire LED diodes, and when I started LED demo I can not start UART in that application. What should I do to get UART functionalities in LED application and vice versa?&lt;BR /&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 08:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-problem/m-p/944521#M54522</guid>
      <dc:creator>mato_cica1</dc:creator>
      <dc:date>2019-07-05T08:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM_KL25Z problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-problem/m-p/944522#M54523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="344171" data-username="mato.cica@gmail.com" href="https://community.nxp.com/people/mato.cica@gmail.com"&gt;Mato Cica&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This question is duplicated with your case, now just add the case answer:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your interest in the NXP kinetis product, I would like to provide service for you.&lt;BR /&gt;Do you configure the correct code?&lt;BR /&gt;Especially the pins, please check the pinmux.c, and refer to the SDK code to add it.&lt;BR /&gt;Then try it again.&lt;BR /&gt;Your problem is mainly caused by your code, please refer to the SDK code carefully.&lt;BR /&gt;If you still have questions about it, please kindly let me know.&lt;BR /&gt;If your question is solved, please tell me to close this case, and help to me fill the feedback as resolved, thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 10:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-problem/m-p/944522#M54523</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-07-05T10:32:08Z</dc:date>
    </item>
  </channel>
</rss>