<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 LPUART module documentation confusing for kinetis k26</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPUART-module-documentation-confusing-for-kinetis-k26/m-p/937429#M54249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In LPUART , in the control register, its already given that bit field 31 and 30 are the &lt;SPAN&gt;R8T9&lt;/SPAN&gt; and &lt;SPAN&gt;R9T8&lt;/SPAN&gt; respectively, which are the received or transmit bits of the data. However,&amp;nbsp;data register of the same module too contains the bits R9T9 and R8T8 which are described as data buffer 9 or 8 for transmit and received. Now comes the confusing part - If I want to write a 10 bit data, where do I write? according to the manual I should first write to CTRL register bits then to the data register bits. But if thats the case, why do we even have the buffer bits in the data register? I also wanted to know the difference between the two, i.e., the R9T9 R8T8 bits of data register and R8T9 R9T8 bits of Control register&lt;/P&gt;&lt;P&gt;&amp;nbsp;I believe I am missing out something here. Any help would be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jul 2019 05:12:02 GMT</pubDate>
    <dc:creator>abhishek_sinha</dc:creator>
    <dc:date>2019-07-04T05:12:02Z</dc:date>
    <item>
      <title>LPUART module documentation confusing for kinetis k26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPUART-module-documentation-confusing-for-kinetis-k26/m-p/937429#M54249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In LPUART , in the control register, its already given that bit field 31 and 30 are the &lt;SPAN&gt;R8T9&lt;/SPAN&gt; and &lt;SPAN&gt;R9T8&lt;/SPAN&gt; respectively, which are the received or transmit bits of the data. However,&amp;nbsp;data register of the same module too contains the bits R9T9 and R8T8 which are described as data buffer 9 or 8 for transmit and received. Now comes the confusing part - If I want to write a 10 bit data, where do I write? according to the manual I should first write to CTRL register bits then to the data register bits. But if thats the case, why do we even have the buffer bits in the data register? I also wanted to know the difference between the two, i.e., the R9T9 R8T8 bits of data register and R8T9 R9T8 bits of Control register&lt;/P&gt;&lt;P&gt;&amp;nbsp;I believe I am missing out something here. Any help would be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 05:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPUART-module-documentation-confusing-for-kinetis-k26/m-p/937429#M54249</guid>
      <dc:creator>abhishek_sinha</dc:creator>
      <dc:date>2019-07-04T05:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART module documentation confusing for kinetis k26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPUART-module-documentation-confusing-for-kinetis-k26/m-p/937430#M54250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Abhishek Sinha,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer the discussion in: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/378121"&gt;LPUART 9 bits data mode&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 06:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPUART-module-documentation-confusing-for-kinetis-k26/m-p/937430#M54250</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-07-05T06:01:30Z</dc:date>
    </item>
  </channel>
</rss>