<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Does flash swap work on chips with FlexNVM?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-flash-swap-work-on-chips-with-FlexNVM/m-p/933517#M54160</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The NXP documentation talks about flash swap not working on chips that have FlexNVM "Enabled".&amp;nbsp; As far as I can tell you can not disable FlexNVM.&amp;nbsp; Does this mean that if you want to use flash swapping that you must use a chip that has only program flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am specifically wondering if it is possible to do flash swapping for firmware update on a MK66FX1M0VLQ18 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 May 2019 21:19:35 GMT</pubDate>
    <dc:creator>c_johnson</dc:creator>
    <dc:date>2019-05-31T21:19:35Z</dc:date>
    <item>
      <title>Does flash swap work on chips with FlexNVM?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-flash-swap-work-on-chips-with-FlexNVM/m-p/933517#M54160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The NXP documentation talks about flash swap not working on chips that have FlexNVM "Enabled".&amp;nbsp; As far as I can tell you can not disable FlexNVM.&amp;nbsp; Does this mean that if you want to use flash swapping that you must use a chip that has only program flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am specifically wondering if it is possible to do flash swapping for firmware update on a MK66FX1M0VLQ18 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 21:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-flash-swap-work-on-chips-with-FlexNVM/m-p/933517#M54160</guid>
      <dc:creator>c_johnson</dc:creator>
      <dc:date>2019-05-31T21:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: Does flash swap work on chips with FlexNVM?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-flash-swap-work-on-chips-with-FlexNVM/m-p/933518#M54161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;No, it is impossible. Please see the reference manual section 4.2&lt;/P&gt;&lt;P&gt;For the devices containing program flash and FlexNVM:&lt;BR /&gt;• The program flash swap feature is not available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2019 07:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-flash-swap-work-on-chips-with-FlexNVM/m-p/933518#M54161</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-06-03T07:56:31Z</dc:date>
    </item>
  </channel>
</rss>