<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKL82Z128VLK7 Factory Parameters in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933307#M54153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;Yes, the slow clock is trimmed by factory. You can see this sentence in page 622 in RM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; A value for SCTRIM is loaded during reset from a factory programmed location.&lt;/P&gt;&lt;P&gt;But there is no word say where is this value location in IFR. I can see in other Kinetis K series device that it's 0x3FF(SCTRIM) and 0x3FE(SCFTRIM). Maybe you can try to use Program Once command to program trim value into this space. But I really don't know if it works.&lt;/P&gt;&lt;P&gt;Another way is use MCUXpresso and P&amp;amp;E as debugger. P&amp;amp;E has additional function to trim 32768 internal osc.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85205i79BA85AA12910E72/image-size/large?v=v2&amp;amp;px=999" title="Untitled1.png" alt="Untitled1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85206iA94CA1918821F73E/image-size/large?v=v2&amp;amp;px=999" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last option is trim by yourself. Then record the value in your code. After reset, you can write this value into register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jun 2019 10:25:15 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-06-03T10:25:15Z</dc:date>
    <item>
      <title>MKL82Z128VLK7 Factory Parameters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933306#M54152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I'm using the internal slow clock of the processor:&lt;/P&gt;&lt;P&gt;after a mass erase of the flash (I'm using Lauterbach) the clock source changed it's&amp;nbsp;&lt;/P&gt;&lt;P&gt;frequency from 32kHz to 40kHz.&lt;/P&gt;&lt;P&gt;I've uploaded the same FW before and after the mass erase.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been looking at the reference manual, I've some questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm me that the internal slow clock source is trimmed by NXP during factory test?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case this answer is yes,&lt;/P&gt;&lt;P&gt;Is possible to load the configuration parameters&amp;nbsp;in order to restore it? In this case, where can I find it in the flash?&lt;/P&gt;&lt;P&gt;Which other parameters are set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 12:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933306#M54152</guid>
      <dc:creator>marcomaioli</dc:creator>
      <dc:date>2019-05-31T12:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: MKL82Z128VLK7 Factory Parameters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933307#M54153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;Yes, the slow clock is trimmed by factory. You can see this sentence in page 622 in RM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; A value for SCTRIM is loaded during reset from a factory programmed location.&lt;/P&gt;&lt;P&gt;But there is no word say where is this value location in IFR. I can see in other Kinetis K series device that it's 0x3FF(SCTRIM) and 0x3FE(SCFTRIM). Maybe you can try to use Program Once command to program trim value into this space. But I really don't know if it works.&lt;/P&gt;&lt;P&gt;Another way is use MCUXpresso and P&amp;amp;E as debugger. P&amp;amp;E has additional function to trim 32768 internal osc.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85205i79BA85AA12910E72/image-size/large?v=v2&amp;amp;px=999" title="Untitled1.png" alt="Untitled1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85206iA94CA1918821F73E/image-size/large?v=v2&amp;amp;px=999" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last option is trim by yourself. Then record the value in your code. After reset, you can write this value into register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2019 10:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933307#M54153</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-06-03T10:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: MKL82Z128VLK7 Factory Parameters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933308#M54154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;thank you very much for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you also provide me the other parameters that are set&amp;nbsp;and can be&amp;nbsp;&lt;/P&gt;&lt;P&gt;erased by a flash mass erase?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2019 15:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933308#M54154</guid>
      <dc:creator>marcomaioli</dc:creator>
      <dc:date>2019-06-04T15:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: MKL82Z128VLK7 Factory Parameters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933309#M54155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry but I haven't. Please check Lauterbach setting. The data in IFR shouldn't be erased during mass erase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 02:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933309#M54155</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-06-05T02:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: MKL82Z128VLK7 Factory Parameters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933310#M54156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 07:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL82Z128VLK7-Factory-Parameters/m-p/933310#M54156</guid>
      <dc:creator>marcomaioli</dc:creator>
      <dc:date>2019-06-05T07:46:18Z</dc:date>
    </item>
  </channel>
</rss>