<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic REGISTER ACCESS IN MCUXPRESSO in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REGISTER-ACCESS-IN-MCUXPRESSO/m-p/930227#M54066</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While programming the FRDM-KV31F board with the MKV31f512vll12 controller using MCUXPRESSO&lt;/P&gt;&lt;P&gt;I need to check if the OSCINIT0 bit in the MCG_S (i.e. Multiplex Clock Generation Status) reg is set. Now I am trying to use the and bitwise operator for the same is there any way I can directly access this bit? I know I can access the Status register via a dot operator as it is a member of the MCG structure, but still is there any way I can directly access the specified bit?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Apurv.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jul 2019 07:02:31 GMT</pubDate>
    <dc:creator>maratheapurv</dc:creator>
    <dc:date>2019-07-17T07:02:31Z</dc:date>
    <item>
      <title>REGISTER ACCESS IN MCUXPRESSO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REGISTER-ACCESS-IN-MCUXPRESSO/m-p/930227#M54066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While programming the FRDM-KV31F board with the MKV31f512vll12 controller using MCUXPRESSO&lt;/P&gt;&lt;P&gt;I need to check if the OSCINIT0 bit in the MCG_S (i.e. Multiplex Clock Generation Status) reg is set. Now I am trying to use the and bitwise operator for the same is there any way I can directly access this bit? I know I can access the Status register via a dot operator as it is a member of the MCG structure, but still is there any way I can directly access the specified bit?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Apurv.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 07:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/REGISTER-ACCESS-IN-MCUXPRESSO/m-p/930227#M54066</guid>
      <dc:creator>maratheapurv</dc:creator>
      <dc:date>2019-07-17T07:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: REGISTER ACCESS IN MCUXPRESSO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/REGISTER-ACCESS-IN-MCUXPRESSO/m-p/930228#M54067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Apurv,&lt;/P&gt;&lt;P&gt;KV31 hardware doesn't support bit access. You can simulate this function by software. For example,&lt;/P&gt;&lt;P&gt;struct GPIO_BITS {&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO0:1;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO1:1;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO2:1;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO3:1;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO4:1;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO5:1;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO6:1;&amp;nbsp;&amp;nbsp; &amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t IO7:1;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t RSVD:8;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// 31:8 Reserved&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;union GPIO_MASK_REG {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; all;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;struct GPIO_BITS&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;bit;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;typedef struct&lt;BR /&gt;{&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;__IO&amp;nbsp;&amp;nbsp; &amp;nbsp;union GPIO_MASK_REG&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ....&lt;/P&gt;&lt;P&gt;}GPIO_TypeDef;&lt;/P&gt;&lt;P&gt;#define&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;GPIOA&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;((GPIO_TypeDef&amp;nbsp;&amp;nbsp; *) GPIOA_BASE )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thus you can access a bit by&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; GPIOA-&amp;gt;MASK.bit.IO7 = 1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 09:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/REGISTER-ACCESS-IN-MCUXPRESSO/m-p/930228#M54067</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-07-17T09:12:03Z</dc:date>
    </item>
  </channel>
</rss>