<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックADC conversion precision</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-conversion-precision/m-p/930161#M54061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm working with the MKE04 with the ADC conversion. I'm reading&amp;nbsp; the signal from a linear potentiometer and I'm trying to differ 100 positions, in this case (0-5v).&lt;/P&gt;&lt;P&gt;The thing is that the ADC conversion is not stable, for example working with 8 bits I get +-4 conversion value when the potentiometer is not moving. I've tried with everything that I know of ( hardware filtering, software average) and I could not get beyond that -+4 value. Then I tried with other board that we have the MKV11Z64 having the vrefh at 5v and the conversion is far better, with just 1 value of error.&lt;/P&gt;&lt;P&gt;The thing is that I cannot use the MKV11 for this project because we are out of space we would like to use a tsop16 micro at best, so I have two questions.&lt;/P&gt;&lt;P&gt;Are there any tsop 16 or less microcontrolers specialised on ADC?&lt;/P&gt;&lt;P&gt;If not, is there any way to improve the adc conversion of my uc?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 May 2019 07:22:58 GMT</pubDate>
    <dc:creator>pauvilanova</dc:creator>
    <dc:date>2019-05-31T07:22:58Z</dc:date>
    <item>
      <title>ADC conversion precision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-conversion-precision/m-p/930161#M54061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm working with the MKE04 with the ADC conversion. I'm reading&amp;nbsp; the signal from a linear potentiometer and I'm trying to differ 100 positions, in this case (0-5v).&lt;/P&gt;&lt;P&gt;The thing is that the ADC conversion is not stable, for example working with 8 bits I get +-4 conversion value when the potentiometer is not moving. I've tried with everything that I know of ( hardware filtering, software average) and I could not get beyond that -+4 value. Then I tried with other board that we have the MKV11Z64 having the vrefh at 5v and the conversion is far better, with just 1 value of error.&lt;/P&gt;&lt;P&gt;The thing is that I cannot use the MKV11 for this project because we are out of space we would like to use a tsop16 micro at best, so I have two questions.&lt;/P&gt;&lt;P&gt;Are there any tsop 16 or less microcontrolers specialised on ADC?&lt;/P&gt;&lt;P&gt;If not, is there any way to improve the adc conversion of my uc?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 07:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-conversion-precision/m-p/930161#M54061</guid>
      <dc:creator>pauvilanova</dc:creator>
      <dc:date>2019-05-31T07:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: ADC conversion precision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-conversion-precision/m-p/930162#M54062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pau,&lt;/P&gt;&lt;P&gt;KE04 ADC shouldn't be so bad.I think you can&lt;/P&gt;&lt;P&gt;1. check VDD power supply. Is there ripple?&lt;/P&gt;&lt;P&gt;2. check Ras/Cas(Figure 16 in datasheet)&lt;/P&gt;&lt;P&gt;3. Please try the ADC example in KE04 SDK to see if the problem caused by hardware or software.&lt;/P&gt;&lt;P&gt;There are some articles shows how to improve adc performance. You can also take a look.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-104288"&gt;https://community.nxp.com/docs/DOC-104288&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN5250&lt;/P&gt;&lt;P&gt;AN4373&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2019 08:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-conversion-precision/m-p/930162#M54062</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-06-04T08:57:43Z</dc:date>
    </item>
  </channel>
</rss>