<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kwikstik audio demo - high noise levels - normal? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235484#M5401</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just got my Kwikstik and ran through the demos.&amp;nbsp; I tried the 2 second audio record demo and plugged my headphones in to hear the playback.&amp;nbsp; The noise level - which sounds like an oscillator running at a few kHz - is very high to the point that it's hard to hear the recorded sound over the noise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wondered about noise coupling in from the PC USB, which shouldn't be a problem, so I tried the demo again with an isolated USB power supply.&amp;nbsp; Same noise levels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this normal?&amp;nbsp; I didn't expect CD quality but even the demo should record reasonable audio quality.&amp;nbsp; It sounds to me like there may be a hardware issue coupling noise into the analog section of this board in which case I need to send it back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody else noticed this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me if this is posted in the wrong place.&amp;nbsp; I assumed there would be a Kwikstik category but didn't find one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 Oct 2013 18:25:55 GMT</pubDate>
    <dc:creator>Scott1487</dc:creator>
    <dc:date>2013-10-26T18:25:55Z</dc:date>
    <item>
      <title>Kwikstik audio demo - high noise levels - normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235484#M5401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just got my Kwikstik and ran through the demos.&amp;nbsp; I tried the 2 second audio record demo and plugged my headphones in to hear the playback.&amp;nbsp; The noise level - which sounds like an oscillator running at a few kHz - is very high to the point that it's hard to hear the recorded sound over the noise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wondered about noise coupling in from the PC USB, which shouldn't be a problem, so I tried the demo again with an isolated USB power supply.&amp;nbsp; Same noise levels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this normal?&amp;nbsp; I didn't expect CD quality but even the demo should record reasonable audio quality.&amp;nbsp; It sounds to me like there may be a hardware issue coupling noise into the analog section of this board in which case I need to send it back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody else noticed this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me if this is posted in the wrong place.&amp;nbsp; I assumed there would be a Kwikstik category but didn't find one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Oct 2013 18:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235484#M5401</guid>
      <dc:creator>Scott1487</dc:creator>
      <dc:date>2013-10-26T18:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: Kwikstik audio demo - high noise levels - normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235485#M5402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As you can see, &lt;STRONG&gt;Kwikstik_Demo&lt;/STRONG&gt; code for &lt;STRONG&gt;Sound_Recorder&lt;/STRONG&gt; is just concept example, the sound quality with this code is not pretty good (I agree with you) but you can create or modify this code in order to improve recording &amp;amp; playing sample for audio signal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 21:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235485#M5402</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-01-13T21:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: Kwikstik audio demo - high noise levels - normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235486#M5403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Scott1487&lt;/P&gt;&lt;P&gt;Standing on hardware design point, TS4974 is a low-power amplifier. So you cannot use this amplifier to drive high-load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 01:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-audio-demo-high-noise-levels-normal/m-p/235486#M5403</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-01-14T01:49:57Z</dc:date>
    </item>
  </channel>
</rss>