<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the max frequency for MCGFFCLK? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928690#M54002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My experience with the FLL is that it will continue to oscillate at its natural resonant frequency when the input reference is removed. When the input is there it will cause it to lock to its value but is not needed for the FLL to actually work.&lt;/P&gt;&lt;P&gt;Presumably using an out of range input is similar to not having one and so it will simply oscillate at its natural frequency instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the FLL output is not used (after transitioning to the final clocking state) it is also not of any real interest what the FLL does.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Oct 2019 10:32:01 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2019-10-17T10:32:01Z</dc:date>
    <item>
      <title>What is the max frequency for MCGFFCLK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928688#M54000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you aren't using the FLL can the MCGFFCLK be configured to be higher than&amp;nbsp;39.0625 kHz?&amp;nbsp; I am using an old mcg driver where pll_init() sets the MCGFFCLK to less than&amp;nbsp;39.0625 kHz even though I am using the PLL not the FLL.&amp;nbsp; The logic is like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt; // the max frequency for the FLL reference is 39.0625kHz so the MCG FF clock should not exceed that&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt; if&amp;nbsp; &amp;nbsp; &amp;nbsp; (crystal_val &amp;lt;= 1250000) {frdiv_val = 0;} // fmax = 1250000/32 = 39062.5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt; else if (crystal_val &amp;lt;= 2500000) {frdiv_val = 1;} // fmax = 2500000/64 = 39062.5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt; else if (crystal_val &amp;lt;= 5000000) ...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't chase down the details in the latest KSDK but I did see this comment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13px; font-family: 'courier new', courier, monospace;"&gt; * When porting to a new board, set the following members&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 13px; font-family: 'courier new', courier, monospace;"&gt; * according to the board setting:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 13px; font-family: 'courier new', courier, monospace;"&gt; * 1. frdiv: If the FLL uses the external reference clock, set this&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 13px; font-family: 'courier new', courier, monospace;"&gt; * value to ensure that the external reference clock divided by frdiv is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 13px; font-family: 'courier new', courier, monospace;"&gt; * in the 31.25 kHz to 39.0625 kHz range.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here it says *if the FLL uses the external reference* - but I am not using the FLL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My MCGFFCLK is 23437.5 Hz but I would like to double it so there is an integer number of cycles per second but then it would exceed 39.0625 kHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2019 17:11:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928688#M54000</guid>
      <dc:creator>matt_boytim</dc:creator>
      <dc:date>2019-10-16T17:11:32Z</dc:date>
    </item>
    <item>
      <title>Re: What is the max frequency for MCGFFCLK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928689#M54001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Matt,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Although you only use the PLL mode, the FLL still be used before being configured into the PLL mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92041iEE3160672E866220/image-size/large?v=v2&amp;amp;px=999" title="MCG mode state diagram.png" alt="MCG mode state diagram.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You must ensure the&amp;nbsp;ffll_ref within FLL reference frequency range.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91612iEB1AC824045B3943/image-size/large?v=v2&amp;amp;px=999" title="FLL reference frequency range.png" alt="FLL reference frequency range.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91732i8DFD05BEC488D950/image-size/large?v=v2&amp;amp;px=999" title="MCG Fixed Frequency Clock.png" alt="MCG Fixed Frequency Clock.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But maybe you can change the frdiv after the MCG has run into PLL? But this is still to be tested.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Best Regards,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Robin&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 08:33:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928689#M54001</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-10-17T08:33:29Z</dc:date>
    </item>
    <item>
      <title>Re: What is the max frequency for MCGFFCLK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928690#M54002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My experience with the FLL is that it will continue to oscillate at its natural resonant frequency when the input reference is removed. When the input is there it will cause it to lock to its value but is not needed for the FLL to actually work.&lt;/P&gt;&lt;P&gt;Presumably using an out of range input is similar to not having one and so it will simply oscillate at its natural frequency instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the FLL output is not used (after transitioning to the final clocking state) it is also not of any real interest what the FLL does.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 10:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928690#M54002</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-10-17T10:32:01Z</dc:date>
    </item>
    <item>
      <title>Re: What is the max frequency for MCGFFCLK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928691#M54003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Robin for the reply.&amp;nbsp; Yeah I would switch FRDIV after the device is already in PEE mode.&amp;nbsp; But the FLL is already disabled in PBE mode:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;The FLL is disabled in a lowpower state.&lt;/P&gt;&lt;P&gt;The FLL reference frequency requirement is clear.&amp;nbsp; But if the FLL is disabled in a lowpower state then it's not clear why it would constrain MCFFCLK.&amp;nbsp; But that is the only spec I can find.&amp;nbsp; I don't like to operate out of spec even if it 'seems' to work although I don't see any reason why it shouldn't.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 13:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928691#M54003</guid>
      <dc:creator>matt_boytim</dc:creator>
      <dc:date>2019-10-18T13:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: What is the max frequency for MCGFFCLK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928692#M54004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;Yeah it doesn't surprise me that that's the case - but in PEE mode the FLL should be disabled in a low power mode so I wasn't concerned what the FLL might do, I was wondering why the MCGFFCLK would still be constrained by the FLL in that case.&amp;nbsp; The requirement on MCGFFCLK is just inferred from its use as fll_ref - but if the FLL is disabled is it 'still' fll_ref and if not then what can it be?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 13:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-the-max-frequency-for-MCGFFCLK/m-p/928692#M54004</guid>
      <dc:creator>matt_boytim</dc:creator>
      <dc:date>2019-10-18T13:50:16Z</dc:date>
    </item>
  </channel>
</rss>