<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Performance analysis and measurement using code warrior 10.4? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Performance-analysis-and-measurement-using-code-warrior-10-4/m-p/235024#M5380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to do advanced performance measurement analysis using code warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using code warrior(eclipse based) v10.4 IDE and our controllers is KL25.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone help me/suggest out with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Anand K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 May 2013 17:38:55 GMT</pubDate>
    <dc:creator>anand-k</dc:creator>
    <dc:date>2013-05-12T17:38:55Z</dc:date>
    <item>
      <title>Performance analysis and measurement using code warrior 10.4?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Performance-analysis-and-measurement-using-code-warrior-10-4/m-p/235024#M5380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to do advanced performance measurement analysis using code warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using code warrior(eclipse based) v10.4 IDE and our controllers is KL25.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone help me/suggest out with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Anand K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 May 2013 17:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Performance-analysis-and-measurement-using-code-warrior-10-4/m-p/235024#M5380</guid>
      <dc:creator>anand-k</dc:creator>
      <dc:date>2013-05-12T17:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: Performance analysis and measurement using code warrior 10.4?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Performance-analysis-and-measurement-using-code-warrior-10-4/m-p/235025#M5381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The KL25 features an on-chip trace buffer (MTB).&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/04/07/first-steps-with-the-pe-tracelink/" title="http://mcuoneclipse.com/2013/04/07/first-steps-with-the-pe-tracelink/"&gt;First Steps with the P&amp;amp;amp;amp;E Tracelink | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/01/13/debugging-arm-cortex-m0-hard-fault-with-mtb-trace/" title="http://mcuoneclipse.com/2013/01/13/debugging-arm-cortex-m0-hard-fault-with-mtb-trace/"&gt;Debugging ARM Cortex-M0+ Hard Fault with MTB Trace | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Based on that trace, the program flow can be analyzed, and the 'SA' part in CodeWarrior can provide performance analysis.&lt;/P&gt;&lt;P&gt;If you are using FreeRTOS, there is FreeRTOS+Trace which gives you performance information:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/03/23/tracing-with-freertostrace-from-percepio/" title="http://mcuoneclipse.com/2012/03/23/tracing-with-freertostrace-from-percepio/"&gt;Tracing with FreeRTOS+Trace from Percepio | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 May 2013 18:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Performance-analysis-and-measurement-using-code-warrior-10-4/m-p/235025#M5381</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-05-12T18:08:11Z</dc:date>
    </item>
  </channel>
</rss>