<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Clock Configuration Issue on MKV58 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-Configuration-Issue-on-MKV58/m-p/915116#M53561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having a trouble with MKV58 clock configuration.&lt;/P&gt;&lt;P&gt;I have a TWR Board and MCU expresso IDE.I simply running "lwip tcp/echo bare metal" example&lt;BR /&gt;without an issue.&lt;/P&gt;&lt;P&gt;However,In my custom board,the example simply stucks in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BOARD_BootClockRUN();" -CLOCK_BootToPeeMode(kMCG_OscselOsc, kMCG_PllClkSelPll0, &amp;amp;mcgConfig_BOARD_BootClockRUN.pll0Config); -CLOCK_SetPbeMode(pllcs, config); -while ((MCG-&amp;gt;S &amp;amp; (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) != (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ve tried to run "Engaded Internal Clock Modes" without an issue,but when it comes to&lt;BR /&gt;run "Engaded External Clock" modes it simply stucks.&lt;/P&gt;&lt;P&gt;In my custom board I have a 50Mhz oscillator which is connected to EXTAL Pin of mcu.&lt;BR /&gt;I observed TWR board and my custom board oscillator inputs,both are the same.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;if i comment &lt;BR /&gt; -while ((MCG-&amp;gt;S &amp;amp; (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) !=&lt;BR /&gt; (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;and /* Disable PLL first, then configure PLL. */&lt;BR /&gt; MCG-&amp;gt;C6 &amp;amp;= ~MCG_C6_PLLS_MASK;&lt;BR /&gt; while (MCG-&amp;gt;S &amp;amp; MCG_S_PLLST_MASK)&lt;BR /&gt; {&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;application gives error in my custom board at&lt;/P&gt;&lt;P&gt;- MCG-&amp;gt;C6 |= MCG_C6_PLLS_MASK;&lt;/P&gt;&lt;P&gt;However, it doesnt happen on TWR Board at all!&lt;/P&gt;&lt;P&gt;So,my questions are,&lt;/P&gt;&lt;P&gt;-Do i miss something to make clock configuration using Clock Config Tools ?&lt;BR /&gt;-What could be the issue ?&lt;BR /&gt;-What else do i need to check ?&lt;/P&gt;&lt;P&gt;King Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2019 12:08:29 GMT</pubDate>
    <dc:creator>softwaretestsof</dc:creator>
    <dc:date>2019-09-26T12:08:29Z</dc:date>
    <item>
      <title>Clock Configuration Issue on MKV58</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-Configuration-Issue-on-MKV58/m-p/915116#M53561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having a trouble with MKV58 clock configuration.&lt;/P&gt;&lt;P&gt;I have a TWR Board and MCU expresso IDE.I simply running "lwip tcp/echo bare metal" example&lt;BR /&gt;without an issue.&lt;/P&gt;&lt;P&gt;However,In my custom board,the example simply stucks in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BOARD_BootClockRUN();" -CLOCK_BootToPeeMode(kMCG_OscselOsc, kMCG_PllClkSelPll0, &amp;amp;mcgConfig_BOARD_BootClockRUN.pll0Config); -CLOCK_SetPbeMode(pllcs, config); -while ((MCG-&amp;gt;S &amp;amp; (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) != (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ve tried to run "Engaded Internal Clock Modes" without an issue,but when it comes to&lt;BR /&gt;run "Engaded External Clock" modes it simply stucks.&lt;/P&gt;&lt;P&gt;In my custom board I have a 50Mhz oscillator which is connected to EXTAL Pin of mcu.&lt;BR /&gt;I observed TWR board and my custom board oscillator inputs,both are the same.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;if i comment &lt;BR /&gt; -while ((MCG-&amp;gt;S &amp;amp; (MCG_S_IREFST_MASK | MCG_S_CLKST_MASK)) !=&lt;BR /&gt; (MCG_S_IREFST(kMCG_FllSrcExternal) | MCG_S_CLKST(kMCG_ClkOutStatExt)))&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;and /* Disable PLL first, then configure PLL. */&lt;BR /&gt; MCG-&amp;gt;C6 &amp;amp;= ~MCG_C6_PLLS_MASK;&lt;BR /&gt; while (MCG-&amp;gt;S &amp;amp; MCG_S_PLLST_MASK)&lt;BR /&gt; {&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;application gives error in my custom board at&lt;/P&gt;&lt;P&gt;- MCG-&amp;gt;C6 |= MCG_C6_PLLS_MASK;&lt;/P&gt;&lt;P&gt;However, it doesnt happen on TWR Board at all!&lt;/P&gt;&lt;P&gt;So,my questions are,&lt;/P&gt;&lt;P&gt;-Do i miss something to make clock configuration using Clock Config Tools ?&lt;BR /&gt;-What could be the issue ?&lt;BR /&gt;-What else do i need to check ?&lt;/P&gt;&lt;P&gt;King Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 12:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-Configuration-Issue-on-MKV58/m-p/915116#M53561</guid>
      <dc:creator>softwaretestsof</dc:creator>
      <dc:date>2019-09-26T12:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: Clock Configuration Issue on MKV58</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-Configuration-Issue-on-MKV58/m-p/915117#M53562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I suggest you should use oscilloscope to measure if the external crystal oscillator has the normal wave.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 01:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-Configuration-Issue-on-MKV58/m-p/915117#M53562</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2019-09-27T01:08:39Z</dc:date>
    </item>
  </channel>
</rss>