<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: More examples on using PWM on the TWR-KV58F220?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/More-examples-on-using-PWM-on-the-TWR-KV58F220/m-p/914908#M53558</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Pls refer to the community:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/508943"&gt;https://community.nxp.com/thread/508943&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jul 2019 06:14:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-07-29T06:14:24Z</dc:date>
    <item>
      <title>More examples on using PWM on the TWR-KV58F220?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/More-examples-on-using-PWM-on-the-TWR-KV58F220/m-p/914907#M53557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently using Mcuxpresso and I have downloaded the corresponding SDK for the board,&lt;/P&gt;&lt;P&gt;after importing the PWM driver example all I get is 3 outputs with different duty cycles,&lt;/P&gt;&lt;P&gt;I get&amp;nbsp; 25%&amp;nbsp; 50% and 70%, curiously the example says 3 phase PWM and the outputs are all in phase.&lt;/P&gt;&lt;P&gt;In the reference manual there is little to almost no information about getting the phase shift configuration,&lt;/P&gt;&lt;P&gt;and the VAL1 to VAL5 registers are all fixed to zero in the example,modifying them is pointless.&lt;/P&gt;&lt;P&gt;I have come across with this many times, the examples are always incomplete.&lt;/P&gt;&lt;P&gt;Can someone please point me to a good reference for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the only page of the reference manual about this mode, so from what I understand VAL4 and VAL5 needs to be modified, but in the example no matter what you do all you get is all of them set to zero.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86079iD546EC2466F099A5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jul 2019 08:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/More-examples-on-using-PWM-on-the-TWR-KV58F220/m-p/914907#M53557</guid>
      <dc:creator>edgardnetz</dc:creator>
      <dc:date>2019-07-28T08:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: More examples on using PWM on the TWR-KV58F220?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/More-examples-on-using-PWM-on-the-TWR-KV58F220/m-p/914908#M53558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Pls refer to the community:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/508943"&gt;https://community.nxp.com/thread/508943&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jul 2019 06:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/More-examples-on-using-PWM-on-the-TWR-KV58F220/m-p/914908#M53558</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-07-29T06:14:24Z</dc:date>
    </item>
  </channel>
</rss>