<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Async Clock Signal in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913649#M53497</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any option that doesnt require adding an additional source?&lt;/P&gt;&lt;P&gt;I dont want to add any more components to the board.&lt;/P&gt;&lt;P&gt;I am running the external 8mhz clock but that's it.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2019 17:45:49 GMT</pubDate>
    <dc:creator>stevenlutz</dc:creator>
    <dc:date>2019-09-26T17:45:49Z</dc:date>
    <item>
      <title>Async Clock Signal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913647#M53495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm making an interface that requires a clock signal output that is 16x the UART baud rate (9600) which puts me at 153.6 kHz.&lt;BR /&gt;I was trying to generate this on the clock out pin but it doesn't seem mathematically possible.&amp;nbsp;&lt;BR /&gt;What other options do i have besides just hitting a gpio port?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is on a MKE18F&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 00:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913647#M53495</guid>
      <dc:creator>stevenlutz</dc:creator>
      <dc:date>2019-09-26T00:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: Async Clock Signal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913648#M53496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Flex Timer may be possible if you have a source that it can use to derive the exact frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Complete Kinetis solutions for professional needs, training and support: &lt;A href="http://www.utasker.com/kinetis.html" target="test_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Kinetis KE1xF:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/FRDM-KE15Z.html" target="test_blank"&gt;http://www.utasker.com/kinetis/FRDM-KE15Z.html&lt;/A&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- &lt;A href="http://www.utasker.com/kinetis/TWR-KE18F.html" target="test_blank"&gt;http://www.utasker.com/kinetis/TWR-KE18F.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&lt;EM&gt;uTasker: supporting &amp;gt;1'000 registered Kinetis users get products faster and cheaper to market&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Request Free emergency remote desk-top consulting at &lt;A href="http://www.utasker.com/services.html" target="test_blank"&gt;http://www.utasker.com/services.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Open Source version at &lt;A href="https://github.com/uTasker/uTasker-Kinetis" target="test_blank"&gt;https://github.com/uTasker/uTasker-Kinetis&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 10:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913648#M53496</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-09-26T10:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: Async Clock Signal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913649#M53497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any option that doesnt require adding an additional source?&lt;/P&gt;&lt;P&gt;I dont want to add any more components to the board.&lt;/P&gt;&lt;P&gt;I am running the external 8mhz clock but that's it.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 17:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913649#M53497</guid>
      <dc:creator>stevenlutz</dc:creator>
      <dc:date>2019-09-26T17:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: Async Clock Signal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913650#M53498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Steven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FTM can be clocked from various sources:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83122i340A3CC28E18770E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you can generate 9600 Baud on the LPUART (with the same clock sources) a x16 clock will also be possible with the same resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 21:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Async-Clock-Signal/m-p/913650#M53498</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-09-26T21:15:56Z</dc:date>
    </item>
  </channel>
</rss>