<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Can I write to Program Once IFR with an external device?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911765#M53438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OTP memory can't be programmed via EzPort.&lt;BR /&gt;It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 May 2019 00:11:18 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2019-05-29T00:11:18Z</dc:date>
    <item>
      <title>Can I write to Program Once IFR with an external device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911764#M53437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;During production, we would like to write serial numbers to the program once field using the SWD connector (or maybe via ezPort?) How do we go about doing that? Is it possible with a PEMicro Cyclone? I think we need an algorithm to access the FCCOB registers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 11:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911764#M53437</guid>
      <dc:creator>atilla</dc:creator>
      <dc:date>2019-05-28T11:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can I write to Program Once IFR with an external device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911765#M53438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OTP memory can't be programmed via EzPort.&lt;BR /&gt;It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 00:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911765#M53438</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-05-29T00:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: Can I write to Program Once IFR with an external device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911766#M53439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Atilla,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Kinetis microcontroller are you working with?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Johnny&lt;/P&gt;&lt;P&gt;PEMicro Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 20:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911766#M53439</guid>
      <dc:creator>johnny_pe</dc:creator>
      <dc:date>2019-06-14T20:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Can I write to Program Once IFR with an external device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911767#M53440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MK64FX512VLL12. Being able to program the PFLASH and DLFASH IFRs will sure come in handy for production. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2019 14:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911767#M53440</guid>
      <dc:creator>atilla</dc:creator>
      <dc:date>2019-06-15T14:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Can I write to Program Once IFR with an external device?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911768#M53441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atilla,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please open a support request on our website. We'll look into adding support for the PFLASH and DFLASH IFRs into our algorithm for the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MK64FX512VLL12&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com"&gt;www.pemicro.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Johnny&lt;/P&gt;&lt;P&gt;PEMicro Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 13:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-write-to-Program-Once-IFR-with-an-external-device/m-p/911768#M53441</guid>
      <dc:creator>johnny_pe</dc:creator>
      <dc:date>2019-06-17T13:36:44Z</dc:date>
    </item>
  </channel>
</rss>