<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis K64 IEEE1588 transmit timestamping</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911012#M53394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know how PTP works, and I looked up FRDM-K64F 1588 bare metal example provided in SDK 2.6.0.&lt;/P&gt;&lt;P&gt;PTP synchronization mechanism between 2 nodes works well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in my project I need to evaluate the accurate propagation delay between 2 nodes, connected via Ethernet cable in a point-to-point configuration.&lt;/P&gt;&lt;P&gt;To do so, I need to know the exact position of timer latching for both transmit and receive packets, in relation to the Ethernet packet or related to TXEN/CRS_DV MAC signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 07:46:46 GMT</pubDate>
    <dc:creator>ombra32</dc:creator>
    <dc:date>2019-08-29T07:46:46Z</dc:date>
    <item>
      <title>Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911010#M53392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;reference manual K64P144M120SF5RM at chapter "45.5.10.3 Receive timestamping" reports that for received frames the Ethernet MAC latches the timer value in correspondence of SFD field.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What happens for transmit frames? When is the timer latched?&lt;/P&gt;&lt;P&gt;This behavior is not explained at relative chapter "45.5.10.2 Transmit timestamping".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 12:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911010#M53392</guid>
      <dc:creator>ombra32</dc:creator>
      <dc:date>2019-08-27T12:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911011#M53393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, this specific timing is not stated in documentation. However, as the Reference Manual indicates, the MAC records the timestamp for the frame in ENETn_ATSTMP. ENETn_EIR[TS_AVAIL] is set to indicate that a new timestamp is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, what it means is that you will have to wait till ENETn_EIR[TS_AVAIL] is set to read the Timestamp of Last Transmitted Frame (ATSTMP).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information I also suggest you to check the following application note regarding IEEE1588 and Kinetis for reference.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4332.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4332.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 15:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911011#M53393</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-08-28T15:52:08Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911012#M53394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know how PTP works, and I looked up FRDM-K64F 1588 bare metal example provided in SDK 2.6.0.&lt;/P&gt;&lt;P&gt;PTP synchronization mechanism between 2 nodes works well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in my project I need to evaluate the accurate propagation delay between 2 nodes, connected via Ethernet cable in a point-to-point configuration.&lt;/P&gt;&lt;P&gt;To do so, I need to know the exact position of timer latching for both transmit and receive packets, in relation to the Ethernet packet or related to TXEN/CRS_DV MAC signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 07:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911012#M53394</guid>
      <dc:creator>ombra32</dc:creator>
      <dc:date>2019-08-29T07:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911013#M53395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to know the exact position of timer latching for both transmit and receive packets, in relation to the Ethernet packet or related to TXEN/CRS_DV MAC signals?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 13:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911013#M53395</guid>
      <dc:creator>ombra32</dc:creator>
      <dc:date>2019-09-05T13:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911014#M53396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anybody help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 10:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911014#M53396</guid>
      <dc:creator>ombra32</dc:creator>
      <dc:date>2019-09-18T10:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911015#M53397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please accept my apologies for my late reply. I will try to ask this internally to see if we can get any feedback.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the inconveniences.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 19:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911015#M53397</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-09-18T19:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911016#M53398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felipe,&lt;/P&gt;&lt;P&gt;any news?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 06:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911016#M53398</guid>
      <dc:creator>ombra32</dc:creator>
      <dc:date>2019-10-07T06:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911017#M53399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have escalated this question with our internal team. I will let you know whenever I received a response. Thanks for your patience.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 19:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911017#M53399</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-10-08T19:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 IEEE1588 transmit timestamping</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911018#M53400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry but this is the only information I could collect from internal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;When user writes the TS bit in Enhanced transmit buffer descriptor field, the Ethernet MAC will timestamp the frame that is ready to transmit and valid when EIR[TS_AVAIL] is set.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2019 20:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-IEEE1588-transmit-timestamping/m-p/911018#M53400</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-10-14T20:30:26Z</dc:date>
    </item>
  </channel>
</rss>