<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MCU for 4.3&amp;quot; TFT Display</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909939#M53334</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the replies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I prefer QFN package, but LQFP it's ok to me. MAPBGA I need at least 4 layer service because the traces are &amp;lt;5 mil. the solder paste is more expensive , T4 instance T3 and is necessary X-Ray inspection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need 800x480 px (no touch) instance of 480x272 because I need use the display in outdoor. The manufacturer of display say me that is not good election 480x272 for outdoor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking to use a display with built lcd controller, SPI, and use a Kinetis K2x or similar.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure but I think that is more easy and cheap to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Sep 2019 09:50:35 GMT</pubDate>
    <dc:creator>jhd</dc:creator>
    <dc:date>2019-09-27T09:50:35Z</dc:date>
    <item>
      <title>MCU for 4.3" TFT Display</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909936#M53331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to select one mcu for use with a 4.3"&amp;nbsp; 480x272 TFT Display (full color).&amp;nbsp;&amp;nbsp;That is able to show the program on the screen in full color and communicate with an MKW41Z via SPI quickly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone TFT display has 24bit-RGB, Parallel MCU, I2C, SPI, UART or USB intefaces, I have not clear which to use.&amp;nbsp;Which do you recommend to use with Kinetis mcu?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And which Kinetis mcu do you recommend for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edited:&amp;nbsp; I have found this doc that is cool&amp;nbsp; &lt;A href="https://www.nxp.com/wcm_documents/techzones/microcontrollers-techzone/Presentations/graphics.lcd.technologies.pdf"&gt;Introduction to graphics and LCD Introduction to graphics and LCD technologies technologies&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not experience with display , I don't know wich interface could simplify development time and BOM. So I'm not sure which interface to choose. I don't need a high resolution, only sometimes show a image but the&amp;nbsp;most of the time the screen shows similar information this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="screen.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85048i4D293DDF78D07552/image-size/large?v=v2&amp;amp;px=999" role="button" title="screen.jpg" alt="screen.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 16:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909936#M53331</guid>
      <dc:creator>jhd</dc:creator>
      <dc:date>2019-09-25T16:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: MCU for 4.3" TFT Display</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909937#M53332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 has an LCD controller that can directly interface to an RGB module (pure TFT without controller needed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are various Kinetis parts with FlexBus that are very efficient with TFTs based on controllers with parallel mode. If highest efficiency is not needed any Kinetis can also bit-bang parallel mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any Kinetis can be used for SPI, I2C or UART connected TFT display with controllers offering these interfaces (or a Kinetis with USB can use a USB device one).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following FTDI display is quite popular for SPI connected devices, based on a controller with graphic accelerator chip which allows simple control and videos etc.(with touch screen control)&amp;nbsp; for simple Kinetis parts.&lt;/P&gt;&lt;P&gt;Here is is shown with a simulated Kinetis part interacting with FTDI's display simulation, which makes development and testing extremely simple:&lt;BR /&gt;&lt;A href="https://www.youtube.com/watch?v=XxC3Y2NaaU8" target="test_blank"&gt;https://www.youtube.com/watch?v=XxC3Y2NaaU8&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis Graphical LCD: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerLCD.PDF" target="test_blank"&gt;http://www.utasker.com/docs/uTasker/uTaskerLCD.PDF&lt;/A&gt;&lt;BR /&gt;Some TFT videos on Kinetis:&lt;BR /&gt;&lt;A href="https://www.youtube.com/watch?v=n-GABeILGV8" target="test_blank"&gt;https://www.youtube.com/watch?v=n-GABeILGV8&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.youtube.com/watch?v=AdtRyQ-2IrE" target="test_blank"&gt;https://www.youtube.com/watch?v=AdtRyQ-2IrE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 21:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909937#M53332</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-09-25T21:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: MCU for 4.3" TFT Display</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909938#M53333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;K70 is a good choice. But I will also recommend LPC54018 and LPC54608. They are NXP new product. The price is very competitive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 08:08:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909938#M53333</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-09-27T08:08:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCU for 4.3" TFT Display</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909939#M53334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the replies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I prefer QFN package, but LQFP it's ok to me. MAPBGA I need at least 4 layer service because the traces are &amp;lt;5 mil. the solder paste is more expensive , T4 instance T3 and is necessary X-Ray inspection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need 800x480 px (no touch) instance of 480x272 because I need use the display in outdoor. The manufacturer of display say me that is not good election 480x272 for outdoor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking to use a display with built lcd controller, SPI, and use a Kinetis K2x or similar.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure but I think that is more easy and cheap to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 09:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909939#M53334</guid>
      <dc:creator>jhd</dc:creator>
      <dc:date>2019-09-27T09:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: MCU for 4.3" TFT Display</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909940#M53335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please check LPC1788FBD144. It is 144 pin LQFP package. LPC54018JBD208E is 208 pin LQFP and it is cheaper. But I think it will also increase your manufacture difficulty.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Sep 2019 02:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-for-4-3-quot-TFT-Display/m-p/909940#M53335</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-09-29T02:07:45Z</dc:date>
    </item>
  </channel>
</rss>