<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Over-voltage-Power-Supply-effects-on-Kinetis-K26-microcontroller/m-p/909709#M53324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Puneeth, &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;No, it won't. Although supply power over 3.6v may harm to the device, it will not change the pin into tri-state or high-impedance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Sep 2019 08:15:59 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-09-12T08:15:59Z</dc:date>
    <item>
      <title>Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Over-voltage-Power-Supply-effects-on-Kinetis-K26-microcontroller/m-p/909708#M53323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using &lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;Kinetis K26 m&lt;/SPAN&gt;icrocontroller&lt;SPAN&gt;&amp;nbsp;in our design. based on the datasheet, supply voltage is 3.3V +/- 10%. in normal operation supply voltage is well with in the mentioned range of 3.3V+/-10%. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However we would like to know the IO's state when power supply range goes&amp;nbsp;above the maximum voltage of 3.6V (maximum of 4.1V).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;will controller retain the previous state of IO's?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;will the state of IO's will be tri-state / High impedance?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Puneeth KB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 06:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Over-voltage-Power-Supply-effects-on-Kinetis-K26-microcontroller/m-p/909708#M53323</guid>
      <dc:creator>puneeth_bheemar</dc:creator>
      <dc:date>2019-09-11T06:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Over-voltage-Power-Supply-effects-on-Kinetis-K26-microcontroller/m-p/909709#M53324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Puneeth, &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;No, it won't. Although supply power over 3.6v may harm to the device, it will not change the pin into tri-state or high-impedance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 08:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Over-voltage-Power-Supply-effects-on-Kinetis-K26-microcontroller/m-p/909709#M53324</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-09-12T08:15:59Z</dc:date>
    </item>
  </channel>
</rss>